<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Fast-mode Plus on i.MX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fast-mode-Plus-on-i-MX6/m-p/315388#M41570</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current I2C specification lists 3 modes of Operation: Standard mode, fast-mode and fast-mode plus. The latter one goes up to 1MHz clock frequency. In the iMX6 reference Manual, I can only find, that the Standard and fast modes are supported. Is that correct or can the i.MX6 be switched into the fast-mode plus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ingo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jun 2014 08:44:55 GMT</pubDate>
    <dc:creator>inmaku</dc:creator>
    <dc:date>2014-06-06T08:44:55Z</dc:date>
    <item>
      <title>Fast-mode Plus on i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-mode-Plus-on-i-MX6/m-p/315388#M41570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current I2C specification lists 3 modes of Operation: Standard mode, fast-mode and fast-mode plus. The latter one goes up to 1MHz clock frequency. In the iMX6 reference Manual, I can only find, that the Standard and fast modes are supported. Is that correct or can the i.MX6 be switched into the fast-mode plus?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ingo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 08:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-mode-Plus-on-i-MX6/m-p/315388#M41570</guid>
      <dc:creator>inmaku</dc:creator>
      <dc:date>2014-06-06T08:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: Fast-mode Plus on i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fast-mode-Plus-on-i-MX6/m-p/315389#M41571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX6 I2C supports standard and fast-mode, but does NOT support the fast-mode plus.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jun 2014 09:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fast-mode-Plus-on-i-MX6/m-p/315389#M41571</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-06-06T09:14:04Z</dc:date>
    </item>
  </channel>
</rss>