<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using SDIO WiFi modules in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315218#M41561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Semih&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at ConnectCard W-i.MX28 module (&lt;SPAN class="st"&gt;Includes &lt;EM&gt;Wi-Fi&lt;/EM&gt;® Access Point mode + &lt;EM&gt;Wi-Fi&lt;/EM&gt; Direct&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.digi.com/pdf/pb_connectcardimx28.pdf"&gt;http://www.digi.com/pdf/pb_connectcardimx28.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.digi.com/support/productdetail?pid=5587&amp;amp;type=documentation" title="http://www.digi.com/support/productdetail?pid=5587&amp;amp;type=documentation"&gt;Documentation for ConnectCard for i.MX28 - Digi International&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jul 2014 00:02:17 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-07-07T00:02:17Z</dc:date>
    <item>
      <title>Using SDIO WiFi modules</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315217#M41560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying find a resource about using SDIO Wi-Fi modules in Linux, either with the mainline kernel or Freescale's old (2.6.35 I believe) kernel. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an example for a board configuration? When I look at other platforms (such as OMAP2) I can see that mmc devices are configured in board files with the driver name (such as wl12xx). But I couldn't figure out how the wireless driver would hook up with the MMC controller in imx28.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Semih&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 18:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315217#M41560</guid>
      <dc:creator>semihhazar</dc:creator>
      <dc:date>2014-07-02T18:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: Using SDIO WiFi modules</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315218#M41561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Semih&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at ConnectCard W-i.MX28 module (&lt;SPAN class="st"&gt;Includes &lt;EM&gt;Wi-Fi&lt;/EM&gt;® Access Point mode + &lt;EM&gt;Wi-Fi&lt;/EM&gt; Direct&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.digi.com/pdf/pb_connectcardimx28.pdf"&gt;http://www.digi.com/pdf/pb_connectcardimx28.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.digi.com/support/productdetail?pid=5587&amp;amp;type=documentation" title="http://www.digi.com/support/productdetail?pid=5587&amp;amp;type=documentation"&gt;Documentation for ConnectCard for i.MX28 - Digi International&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jul 2014 00:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315218#M41561</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-07T00:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: Using SDIO WiFi modules</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315219#M41562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Well here's how it works if somebody is also puzzled like me:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You don't need something special in the DTS or board config file to hook a certain SDIO device with a driver. Once the MMC system is up it does a scan on the bus and creates a device with the correct id and then kernel tries to match this device with an appropriate driver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2014 08:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-SDIO-WiFi-modules/m-p/315219#M41562</guid>
      <dc:creator>semihhazar</dc:creator>
      <dc:date>2014-07-11T08:14:00Z</dc:date>
    </item>
  </channel>
</rss>