<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Debugging U-boot on iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315154#M41550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the pointers.&lt;/P&gt;&lt;P&gt;I had looked at some of these options but not all.&lt;/P&gt;&lt;P&gt;I’ll set up something in the next few weeks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jun 2014 16:26:30 GMT</pubDate>
    <dc:creator>mg</dc:creator>
    <dc:date>2014-06-10T16:26:30Z</dc:date>
    <item>
      <title>Debugging U-boot on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315152#M41548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to know what options are available for source level debugging of U-boot for the iMX6 processor (Quad or Solo).&lt;/P&gt;&lt;P&gt;I have a custom board using iMX6S and the design for this board is based on the Sabre SD reference board which uses iMX6Q.&lt;/P&gt;&lt;P&gt;To begin with, I would like to setup the environment to debug U-boot for the Sabre SD board.&lt;/P&gt;&lt;P&gt;I can then use this as the basis for setting up the debug environment for my custom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my current setup:&lt;/P&gt;&lt;P&gt;- Reference board used: Sabre SD board - MCIMX6Q SDB&lt;/P&gt;&lt;P&gt;- Kernel version: LTIB Linux 3.0.35&lt;/P&gt;&lt;P&gt;- U-boot version: 2009.08&lt;/P&gt;&lt;P&gt;I have a bootable SD card that has all the binaries (U-boot, kernel and rootfs) and I can bring up the Sabre board with these binaries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So now, I would like to modify U-boot for my custom board and hence would like to have a debugging environment that allows for single stepping.&lt;/P&gt;&lt;P&gt;Has anyone tried using J-link? If yes, what was the setup (use Eclipse for building U-boot and then use JTAG for debugging)?&lt;/P&gt;&lt;P&gt;Any pointers here will be very helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;MG.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 23:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315152#M41548</guid>
      <dc:creator>mg</dc:creator>
      <dc:date>2014-06-05T23:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging U-boot on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315153#M41549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi M G&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think subject well described on various links below, please&lt;/P&gt;&lt;P&gt;look at them&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://support.bluetechnix.at/wiki/ARM_DS-5_Quick_Start_%28i.MX6%29" title="https://support.bluetechnix.at/wiki/ARM_DS-5_Quick_Start_%28i.MX6%29"&gt;ARM DS-5 Quick Start (i.MX6) - BlueWiki&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/305186"&gt;OpenOCD Problem i.MX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309446"&gt;Load u-boot with JTAG&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550" title="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1550"&gt;Getting J-Link working with i.MX6Q - J-Link/Flasher related - SEGGER Forum&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1734" title="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1734"&gt;Problems debugging I.MX6 with J-Link and GDB-Server - J-Link/Flasher related - SEGGER Forum&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1590" title="http://forum.segger.com/index.php?page=Thread&amp;amp;threadID=1590"&gt;Freescale imx6 sabre lite support in jlink software version 4.58a - J-Link/Flasher related - SEGGER Forum&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation"&gt;AN4553&lt;/A&gt; Using Open Source Debugging Tools for Linux on i.MX Processors&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jun 2014 07:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315153#M41549</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-09T07:14:26Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging U-boot on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315154#M41550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the pointers.&lt;/P&gt;&lt;P&gt;I had looked at some of these options but not all.&lt;/P&gt;&lt;P&gt;I’ll set up something in the next few weeks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 16:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-U-boot-on-iMX6/m-p/315154#M41550</guid>
      <dc:creator>mg</dc:creator>
      <dc:date>2014-06-10T16:26:30Z</dc:date>
    </item>
  </channel>
</rss>