<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: For DDR Memory word size 64 bits, which clock is connected upper 32 bits  and which clock is connected lower 32 bits</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/For-DDR-Memory-word-size-64-bits-which-clock-is-connected-upper/m-p/314886#M41490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As for DRAM clocks : in default state both signals are the same and can be used for both (any) &lt;/P&gt;&lt;P&gt;CS0 or CS1 if this makes easier PCB design.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jul 2014 07:41:02 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-07-02T07:41:02Z</dc:date>
    <item>
      <title>For DDR Memory word size 64 bits, which clock is connected upper 32 bits  and which clock is connected lower 32 bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/For-DDR-Memory-word-size-64-bits-which-clock-is-connected-upper/m-p/314885#M41489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All,&lt;/P&gt;&lt;P&gt;we need to achieve 64 bits word size. we are using 4 memory chips of 256MX16.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6 processor is generating two pairs of differentail clocks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;out of two pairs generated by processor which pair of the clock we need to connected Memory chips and what is the purpose of two pairs of differentail clocks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 07:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/For-DDR-Memory-word-size-64-bits-which-clock-is-connected-upper/m-p/314885#M41489</guid>
      <dc:creator>muralikrishna</dc:creator>
      <dc:date>2014-07-02T07:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: For DDR Memory word size 64 bits, which clock is connected upper 32 bits  and which clock is connected lower 32 bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/For-DDR-Memory-word-size-64-bits-which-clock-is-connected-upper/m-p/314886#M41490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As for DRAM clocks : in default state both signals are the same and can be used for both (any) &lt;/P&gt;&lt;P&gt;CS0 or CS1 if this makes easier PCB design.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 07:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/For-DDR-Memory-word-size-64-bits-which-clock-is-connected-upper/m-p/314886#M41490</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-07-02T07:41:02Z</dc:date>
    </item>
  </channel>
</rss>