<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Yocto media player using hardware decoder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-player-using-hardware-decoder/m-p/314839#M41467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to run some HD video on the i.mx6 SOLO in Yocto.&lt;/P&gt;&lt;P&gt;I tried the qt-media player and the "video" player that is build in in Yocto-x11, the CPU load runs up to around 30% when the video is playing.&lt;/P&gt;&lt;P&gt;However, when i use gst-launch command (gstreamer) through console, the CPU load is less than 10%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the above, i would think that the qt-media player and the "video" player in the Yocto is using software decoder, while gstreamer is using hardware decoder, and thus has the difference in CPU load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyway we can get the qt-media player to use the hardware decoder? Or is there any player for Yocto that utilise the hardware decoder like gstreamer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Zhen Cong Tee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jul 2014 07:20:19 GMT</pubDate>
    <dc:creator>zhencongtee</dc:creator>
    <dc:date>2014-07-02T07:20:19Z</dc:date>
    <item>
      <title>Yocto media player using hardware decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-player-using-hardware-decoder/m-p/314839#M41467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to run some HD video on the i.mx6 SOLO in Yocto.&lt;/P&gt;&lt;P&gt;I tried the qt-media player and the "video" player that is build in in Yocto-x11, the CPU load runs up to around 30% when the video is playing.&lt;/P&gt;&lt;P&gt;However, when i use gst-launch command (gstreamer) through console, the CPU load is less than 10%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the above, i would think that the qt-media player and the "video" player in the Yocto is using software decoder, while gstreamer is using hardware decoder, and thus has the difference in CPU load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyway we can get the qt-media player to use the hardware decoder? Or is there any player for Yocto that utilise the hardware decoder like gstreamer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Zhen Cong Tee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 07:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-player-using-hardware-decoder/m-p/314839#M41467</guid>
      <dc:creator>zhencongtee</dc:creator>
      <dc:date>2014-07-02T07:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto media player using hardware decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-player-using-hardware-decoder/m-p/314840#M41468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately there is not a hardware decoder option available for the qt-media player right now. Only gstreamer allows for this option as of today.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 20:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-player-using-hardware-decoder/m-p/314840#M41468</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2014-07-08T20:05:22Z</dc:date>
    </item>
  </channel>
</rss>