<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can I use DMA in DM Core? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-DMA-in-DM-Core/m-p/314653#M41394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see DMA block in "DM Core Block Diagram".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This diagram is on "i.MX6D/Q Reference Manual".&lt;/P&gt;&lt;P&gt;The figure is "Figure 48-1. DM Core Block Diagram" at p.4054 in the Reference Manual Rev. 1, 04/2013.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use this DMA in DM Core?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe that this DMA can be used in EP mode at least.&lt;/P&gt;&lt;P&gt;But there is no details in the Reference Manual regarding above matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to thank if you can show me the relevant document or the specification for the DMA in DM Core?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hiromichi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jun 2014 06:14:52 GMT</pubDate>
    <dc:creator>hiromichimatsum</dc:creator>
    <dc:date>2014-06-05T06:14:52Z</dc:date>
    <item>
      <title>Can I use DMA in DM Core?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-DMA-in-DM-Core/m-p/314653#M41394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see DMA block in "DM Core Block Diagram".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This diagram is on "i.MX6D/Q Reference Manual".&lt;/P&gt;&lt;P&gt;The figure is "Figure 48-1. DM Core Block Diagram" at p.4054 in the Reference Manual Rev. 1, 04/2013.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use this DMA in DM Core?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe that this DMA can be used in EP mode at least.&lt;/P&gt;&lt;P&gt;But there is no details in the Reference Manual regarding above matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to thank if you can show me the relevant document or the specification for the DMA in DM Core?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hiromichi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 06:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-DMA-in-DM-Core/m-p/314653#M41394</guid>
      <dc:creator>hiromichimatsum</dc:creator>
      <dc:date>2014-06-05T06:14:52Z</dc:date>
    </item>
  </channel>
</rss>