<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 QT on the SABRE for eReaders</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QT-on-the-SABRE-for-eReaders/m-p/164535#M4136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am delving into the embedded software market and I am looking to purchase a SABRE eReader in the near future.&amp;nbsp; I am a software developer and never done anything to do with hardware devices, so I am finding all this a steep learning curve.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking to develop an application that runs on the SABRE eReader that uses its touch and e-ink display.&amp;nbsp; (By the way what is the difference between SABRE AND SABRE2, apart from the cost :smileyhappy: ).&amp;nbsp; However before I put down the $1000 I wanted to get a head start on developing the software using QT.&amp;nbsp; I have looked at a few posts that explain how to get QT running, but they all seem to be for a normal lcd/led display.&amp;nbsp; So my questions are&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Can I use the QT SDK to control the e-ink display.&amp;nbsp; I know on the kindle this had to be done via C directly.&amp;nbsp; Have freescale got some kind of interface?&lt;/P&gt;&lt;P&gt;2) Can I also use the QT SDK to record the touch interface on the e-ink display.&lt;/P&gt;&lt;P&gt;3) Would anyone advise against using QT to develop this e-ink touch application?&amp;nbsp; If so what alternatives do I have.&lt;/P&gt;&lt;P&gt;4) Is there another version of the SABRE eReader coming out soon, if so what is the timescale?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I have not dealt with different CPU architectures before now, how do people generally develop applications.&amp;nbsp; Do they do all the development and compilation on the reference board, or do they use a normal i386 pc and some kind of emulator, and when they are ready to test it on the board they compile it on the board and run it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and sorry for the noob questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Hamza Khan-Cheema&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Nov 2012 17:33:08 GMT</pubDate>
    <dc:creator>hamzakc</dc:creator>
    <dc:date>2012-11-05T17:33:08Z</dc:date>
    <item>
      <title>QT on the SABRE for eReaders</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-on-the-SABRE-for-eReaders/m-p/164535#M4136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am delving into the embedded software market and I am looking to purchase a SABRE eReader in the near future.&amp;nbsp; I am a software developer and never done anything to do with hardware devices, so I am finding all this a steep learning curve.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking to develop an application that runs on the SABRE eReader that uses its touch and e-ink display.&amp;nbsp; (By the way what is the difference between SABRE AND SABRE2, apart from the cost :smileyhappy: ).&amp;nbsp; However before I put down the $1000 I wanted to get a head start on developing the software using QT.&amp;nbsp; I have looked at a few posts that explain how to get QT running, but they all seem to be for a normal lcd/led display.&amp;nbsp; So my questions are&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Can I use the QT SDK to control the e-ink display.&amp;nbsp; I know on the kindle this had to be done via C directly.&amp;nbsp; Have freescale got some kind of interface?&lt;/P&gt;&lt;P&gt;2) Can I also use the QT SDK to record the touch interface on the e-ink display.&lt;/P&gt;&lt;P&gt;3) Would anyone advise against using QT to develop this e-ink touch application?&amp;nbsp; If so what alternatives do I have.&lt;/P&gt;&lt;P&gt;4) Is there another version of the SABRE eReader coming out soon, if so what is the timescale?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I have not dealt with different CPU architectures before now, how do people generally develop applications.&amp;nbsp; Do they do all the development and compilation on the reference board, or do they use a normal i386 pc and some kind of emulator, and when they are ready to test it on the board they compile it on the board and run it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and sorry for the noob questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Hamza Khan-Cheema&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2012 17:33:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-on-the-SABRE-for-eReaders/m-p/164535#M4136</guid>
      <dc:creator>hamzakc</dc:creator>
      <dc:date>2012-11-05T17:33:08Z</dc:date>
    </item>
  </channel>
</rss>