<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mx28 Where is uboot sourcecode in LTIB? Thanks! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314443#M41342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I´ve been using u-boot from &lt;A href="https://github.com/Freescale/u-boot-fslc" title="https://github.com/Freescale/u-boot-fslc"&gt;Freescale/u-boot-fslc · GitHub&lt;/A&gt;, branch name patches-2014.01, but this u-boot does not need bootlets, if it´s a requirement for you it will not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you want to "taste" this u-boot, you can download this pre-built image:&lt;/P&gt;&lt;P&gt;&lt;A href="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard" title="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard"&gt;http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-201405…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;from&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/" title="http://freescale.github.io/"&gt;FSL Community BSP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it´s a framebuffer image. You can copy it to a sdcard using:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ sudo dd if=fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard of=/dev/sdX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jun 2014 15:21:22 GMT</pubDate>
    <dc:creator>daiane_angolini</dc:creator>
    <dc:date>2014-06-05T15:21:22Z</dc:date>
    <item>
      <title>mx28 Where is uboot sourcecode in LTIB? Thanks!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314439#M41338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,all&lt;/P&gt;&lt;P&gt;I have install LTIB,and compile ok.&lt;/P&gt;&lt;P&gt;there is imx28_ivt_uboot.sb and imx28_ivt_linux.sb in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rootfs/boot/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can find linux-2.6.35 sourcecode in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rpm/BUILD.&lt;/P&gt;&lt;P&gt;I can find imx-bootlets-src-2.6.35.3-1.1.0 sourcecode in the /opt/i.mx28x/L2.6.35_1.1.0_130130_source/source/ltib/rpm/BUILD.&lt;/P&gt;&lt;P&gt;I need to modify some uboot sourcecode,but where is uboot sourcecode??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 01:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314439#M41338</guid>
      <dc:creator>HaohuaQIN</dc:creator>
      <dc:date>2014-06-05T01:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: mx28 Where is uboot sourcecode in LTIB? Thanks!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314440#M41339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;you can try: &lt;SPAN style="text-decoration: underline;"&gt;./ltib -m prep -p u-boot&lt;/SPAN&gt; to prepare the u-boot package, then you will find u-boot source codes in ltib/rpm/Build/u-boot...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 01:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314440#M41339</guid>
      <dc:creator>tonyzheng</dc:creator>
      <dc:date>2014-06-05T01:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: mx28 Where is uboot sourcecode in LTIB? Thanks!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314441#M41340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 浩华，&lt;/P&gt;&lt;P&gt;As Jimse has told you that use the commend:&lt;STRONG&gt;./ltib -m prep -p u-boot&lt;/STRONG&gt; under ltib directory, you will find the source code.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 01:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314441#M41340</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-06-05T01:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: mx28 Where is uboot sourcecode in LTIB? Thanks!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314442#M41341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you very much!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 12:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314442#M41341</guid>
      <dc:creator>HaohuaQIN</dc:creator>
      <dc:date>2014-06-05T12:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: mx28 Where is uboot sourcecode in LTIB? Thanks!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314443#M41342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I´ve been using u-boot from &lt;A href="https://github.com/Freescale/u-boot-fslc" title="https://github.com/Freescale/u-boot-fslc"&gt;Freescale/u-boot-fslc · GitHub&lt;/A&gt;, branch name patches-2014.01, but this u-boot does not need bootlets, if it´s a requirement for you it will not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you want to "taste" this u-boot, you can download this pre-built image:&lt;/P&gt;&lt;P&gt;&lt;A href="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard" title="http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard"&gt;http://ci.ossystems.com.br/public/fsl-community-bsp/daisy/12/framebuffer/imx28evk/fsl-image-machine-test-imx28evk-201405…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;from&lt;/P&gt;&lt;P&gt;&lt;A href="http://freescale.github.io/" title="http://freescale.github.io/"&gt;FSL Community BSP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it´s a framebuffer image. You can copy it to a sdcard using:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ sudo dd if=fsl-image-machine-test-imx28evk-20140523-12.rootfs.sdcard of=/dev/sdX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jun 2014 15:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mx28-Where-is-uboot-sourcecode-in-LTIB-Thanks/m-p/314443#M41342</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2014-06-05T15:21:22Z</dc:date>
    </item>
  </channel>
</rss>