<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how to debug the kernel when it stops at kernel booting? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-debug-the-kernel-when-it-stops-at-kernel-booting/m-p/164471#M4126</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had hoped there would be some help from Freescale if nobody elese could answer a question. Clearly this is not the case.&lt;/P&gt;&lt;P&gt;Any how I would like to share my pregress.&lt;/P&gt;&lt;P&gt;If configuring through the linux configuration menu, turning on Low Level Debug will cause compiling error. This is there is&amp;nbsp;no switch for this in debug.s (under kernel) without selecting ICE debug, which I don't have. My solution to this is hard code the definition of MXC_LL_UART_PADDR and MXC_LL_UART_VADDR to files asking for it. By this I got debug information until MMU is enabled.&lt;/P&gt;&lt;P&gt;My problem is now the kernel hangs after MMU is&amp;nbsp;enabled and before booting information comes out. Anybody can give me some clues? Any comments will be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Aug 2011 16:24:19 GMT</pubDate>
    <dc:creator>jlu</dc:creator>
    <dc:date>2011-08-24T16:24:19Z</dc:date>
    <item>
      <title>how to debug the kernel when it stops at kernel booting?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-debug-the-kernel-when-it-stops-at-kernel-booting/m-p/164470#M4125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;﻿I've a custom designed i.mx25 board. the board has nothing except a CAN, 2G NAND, 64MB DDR2, UART, some buttons, a clone to the 3 stack board for what it has. One PCB loads the kernel all right, another PCB, which is the 2nd layout and supposely better one, stops after "decompressing... done. booting kernel". I tried all kinds of kernel configuration in order to trace down where the problem comes from, but none gives me more info. among the configurations I've tried, "low-level debug functions" had caused periodic reset, "debug shared IRQ handlers" and "detect soft lockups" had caused unrecognisable bad data crc image file.&lt;/P&gt;&lt;P&gt;how can i trace down the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2011 03:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-debug-the-kernel-when-it-stops-at-kernel-booting/m-p/164470#M4125</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2011-08-04T03:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: how to debug the kernel when it stops at kernel booting?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-debug-the-kernel-when-it-stops-at-kernel-booting/m-p/164471#M4126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had hoped there would be some help from Freescale if nobody elese could answer a question. Clearly this is not the case.&lt;/P&gt;&lt;P&gt;Any how I would like to share my pregress.&lt;/P&gt;&lt;P&gt;If configuring through the linux configuration menu, turning on Low Level Debug will cause compiling error. This is there is&amp;nbsp;no switch for this in debug.s (under kernel) without selecting ICE debug, which I don't have. My solution to this is hard code the definition of MXC_LL_UART_PADDR and MXC_LL_UART_VADDR to files asking for it. By this I got debug information until MMU is enabled.&lt;/P&gt;&lt;P&gt;My problem is now the kernel hangs after MMU is&amp;nbsp;enabled and before booting information comes out. Anybody can give me some clues? Any comments will be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2011 16:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-debug-the-kernel-when-it-stops-at-kernel-booting/m-p/164471#M4126</guid>
      <dc:creator>jlu</dc:creator>
      <dc:date>2011-08-24T16:24:19Z</dc:date>
    </item>
  </channel>
</rss>