<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Run and Debug problems</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Run-and-Debug-problems/m-p/313228#M41050</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&amp;nbsp; I'm using i.mx53 jumpstart kit. I have a new problem, I have configured the network using DCHP, I used the ping command and the connection works very well, but when I try to&amp;nbsp; debug&amp;nbsp; the application it goes wrong, the console display that the connection is refused and the remote console don't show&amp;nbsp; anything, I have attached the screenshots of the Run configuration Display and Debug configurations display, Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.D.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Ubuntu 12.04&amp;nbsp; on a native PC, wired local network and serial USB converter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Apr 2014 23:10:46 GMT</pubDate>
    <dc:creator>jacoblòpez</dc:creator>
    <dc:date>2014-04-09T23:10:46Z</dc:date>
    <item>
      <title>Run and Debug problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Run-and-Debug-problems/m-p/313228#M41050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&amp;nbsp; I'm using i.mx53 jumpstart kit. I have a new problem, I have configured the network using DCHP, I used the ping command and the connection works very well, but when I try to&amp;nbsp; debug&amp;nbsp; the application it goes wrong, the console display that the connection is refused and the remote console don't show&amp;nbsp; anything, I have attached the screenshots of the Run configuration Display and Debug configurations display, Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.D.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Ubuntu 12.04&amp;nbsp; on a native PC, wired local network and serial USB converter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 23:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Run-and-Debug-problems/m-p/313228#M41050</guid>
      <dc:creator>jacoblòpez</dc:creator>
      <dc:date>2014-04-09T23:10:46Z</dc:date>
    </item>
  </channel>
</rss>