<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Tamper function in i.MX6. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313126#M41033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although the IMX6 chip supports the tamper function, but we haven't connected the tamper detection pin to IOMUX pad, so the function can't be used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Apr 2014 03:08:49 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2014-04-10T03:08:49Z</dc:date>
    <item>
      <title>Tamper function in i.MX6.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313125#M41032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like the sample code of Tamper function for i.MX6.&lt;/P&gt;&lt;P&gt;Does the sample code exist?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 00:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313125#M41032</guid>
      <dc:creator>keitanagashima</dc:creator>
      <dc:date>2014-04-10T00:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: Tamper function in i.MX6.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313126#M41033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although the IMX6 chip supports the tamper function, but we haven't connected the tamper detection pin to IOMUX pad, so the function can't be used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 03:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313126#M41033</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-04-10T03:08:49Z</dc:date>
    </item>
    <item>
      <title>Re: Tamper function in i.MX6.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313127#M41034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Qiang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I'd like to use tamper detection for Voltage, Temperature, SRTC, Wire mesh.&lt;/P&gt;&lt;P&gt;Are these features supported by i.MX6?&lt;/P&gt;&lt;P&gt;If it is supported, give me sample code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keita &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 03:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313127#M41034</guid>
      <dc:creator>keitanagashima</dc:creator>
      <dc:date>2014-04-10T03:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Tamper function in i.MX6.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313128#M41035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think they can't be supported.&lt;/P&gt;&lt;P&gt;The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).&lt;/P&gt;&lt;P&gt;But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 05:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Tamper-function-in-i-MX6/m-p/313128#M41035</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-04-10T05:21:34Z</dc:date>
    </item>
  </channel>
</rss>