<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PMIC SWBSTFB Max Rating in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312973#M40998</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SWBSTFB max rating voltage is only 4.8V in the PF0100 data sheet (page 9).&lt;/P&gt;&lt;P&gt;It's a little bit surprising as the boost output voltage can go up to 5,15V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Apr 2014 10:07:26 GMT</pubDate>
    <dc:creator>danielkubiak</dc:creator>
    <dc:date>2014-04-09T10:07:26Z</dc:date>
    <item>
      <title>PMIC SWBSTFB Max Rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312973#M40998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SWBSTFB max rating voltage is only 4.8V in the PF0100 data sheet (page 9).&lt;/P&gt;&lt;P&gt;It's a little bit surprising as the boost output voltage can go up to 5,15V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 10:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312973#M40998</guid>
      <dc:creator>danielkubiak</dc:creator>
      <dc:date>2014-04-09T10:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC SWBSTFB Max Rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312974#M40999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 17:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312974#M40999</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2014-04-09T17:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC SWBSTFB Max Rating</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312975#M41000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 07:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-SWBSTFB-Max-Rating/m-p/312975#M41000</guid>
      <dc:creator>danielkubiak</dc:creator>
      <dc:date>2014-04-10T07:53:39Z</dc:date>
    </item>
  </channel>
</rss>