<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック/dev/spidev not appearing on iMX6Q despite kernel configuration and modalias=&amp;quot;spidev&amp;quot;</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312729#M40968</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using iMX6Q with BSP L3.0.35_4.1.0.&lt;/P&gt;&lt;P&gt;I configured the kernel in imx6_defconfig.dev as &lt;/P&gt;&lt;P&gt;CONFIG_SPI_SPI_DEV=y&amp;nbsp; &lt;/P&gt;&lt;P&gt;CONFIG_SPI=y&lt;/P&gt;&lt;P&gt;CONFIG_SPI_MASTER=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the /arch/arm/mach-mx6/board-*.c file. &lt;/P&gt;&lt;P&gt;I did the following changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;IOMUX for chip select.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static int mx6q_spi_cs[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -1, IS THIS A PROMLEM? I want to use SS of ecspi.&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;static const struct spi_imx_master e25_mx6q_spi_data __initconst = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .chipselect&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = e25_mx6q_spi_cs,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .num_chipselect = ARRAY_SIZE(e25_mx6q_spi_cs),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;static struct spi_board_info my_spi5_board_info[] __initdata = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* The modalias must be the same as spi device driver name */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .modalias&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "spidev",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .max_speed_hz&amp;nbsp;&amp;nbsp; = 10000000,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bus_num&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .chip_select&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .platform_data&amp;nbsp; = NULL,I&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; },&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx6q_add_ecspi(4, &amp;amp;mx6q_spi_data);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; spi_device_init();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to configure CS a GPIO nd gave teh corresponding GPIO number in the mc6q_spi_cs struct. But not luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers would be very helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Apr 2014 16:21:11 GMT</pubDate>
    <dc:creator>muthuswamydiksh</dc:creator>
    <dc:date>2014-04-08T16:21:11Z</dc:date>
    <item>
      <title>/dev/spidev not appearing on iMX6Q despite kernel configuration and modalias="spidev"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312729#M40968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using iMX6Q with BSP L3.0.35_4.1.0.&lt;/P&gt;&lt;P&gt;I configured the kernel in imx6_defconfig.dev as &lt;/P&gt;&lt;P&gt;CONFIG_SPI_SPI_DEV=y&amp;nbsp; &lt;/P&gt;&lt;P&gt;CONFIG_SPI=y&lt;/P&gt;&lt;P&gt;CONFIG_SPI_MASTER=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the /arch/arm/mach-mx6/board-*.c file. &lt;/P&gt;&lt;P&gt;I did the following changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;IOMUX for chip select.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static int mx6q_spi_cs[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -1, IS THIS A PROMLEM? I want to use SS of ecspi.&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;static const struct spi_imx_master e25_mx6q_spi_data __initconst = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .chipselect&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = e25_mx6q_spi_cs,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .num_chipselect = ARRAY_SIZE(e25_mx6q_spi_cs),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;static struct spi_board_info my_spi5_board_info[] __initdata = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* The modalias must be the same as spi device driver name */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .modalias&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "spidev",&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .max_speed_hz&amp;nbsp;&amp;nbsp; = 10000000,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bus_num&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .chip_select&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .platform_data&amp;nbsp; = NULL,I&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; },&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx6q_add_ecspi(4, &amp;amp;mx6q_spi_data);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; spi_device_init();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to configure CS a GPIO nd gave teh corresponding GPIO number in the mc6q_spi_cs struct. But not luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers would be very helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 16:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312729#M40968</guid>
      <dc:creator>muthuswamydiksh</dc:creator>
      <dc:date>2014-04-08T16:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: /dev/spidev not appearing on iMX6Q despite kernel configuration and modalias="spidev"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312730#M40969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I referred:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/307257"&gt;spidev&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/316764"&gt;how open spidev on imx28 platform?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But still it is not appearing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 16:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312730#M40969</guid>
      <dc:creator>muthuswamydiksh</dc:creator>
      <dc:date>2014-04-08T16:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: /dev/spidev not appearing on iMX6Q despite kernel configuration and modalias="spidev"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312731#M40970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A href="https://community.nxp.com/space/2004"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 09:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312731#M40970</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-04-09T09:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: /dev/spidev not appearing on iMX6Q despite kernel configuration and modalias="spidev"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312732#M40971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Move the post to i.MX Commnity.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The port pin has to be correctly configured for the required chip select in IOMUX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The array has to be:&lt;/P&gt;&lt;P&gt;static int mx6q_spi_cs[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; -1, &lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;three -1s are required here as i am using CS2. If you dig more into kernel spi code, you will find that size of the array mx6q_spi_cs has to be greater than your .chip_select field. With these changes, I can see /dev/spi4.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Apr 2014 10:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/dev-spidev-not-appearing-on-iMX6Q-despite-kernel-configuration/m-p/312732#M40971</guid>
      <dc:creator>muthuswamydiksh</dc:creator>
      <dc:date>2014-04-26T10:26:00Z</dc:date>
    </item>
  </channel>
</rss>