<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: spidev on sabrelite in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/spidev-on-sabrelite/m-p/312320#M40895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the only SPI device on the SABRE Lite (BD-SL-i.MX6) is the SPI-NOR flash, we don't enable userspace SPI in our default configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can enable it using the kernel's "menuconfig" or by adding "CONFIG_SPI_SPIDEV=y" to your kernel configuration, but the SPI-NOR is accessible using the MTD driver, so SPIDEV isn't needed for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on a configuration that will re-purpose the LCD connector (J15) on the SABRE Lite boards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can enable it using the kernel's "menuconfig" or by adding "CONFIG_SPI_SPIDEV=y" to your kernel configuration, but the SPI-NOR is accessible using the MTD driver, so SPIDEV isn't needed for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on customer feedback, we are working on a configuration that will re-purpose the LCD connector (J15) on the SABRE Lite boards as a combination of GPIO and additional SPI channels (ECSPI2/3).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 May 2014 14:17:10 GMT</pubDate>
    <dc:creator>EricNelson</dc:creator>
    <dc:date>2014-05-08T14:17:10Z</dc:date>
    <item>
      <title>spidev on sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/spidev-on-sabrelite/m-p/312319#M40894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using sabrelite board with 2009.08 u-boot and 3.0.35 linux kernel (LTIB BSP) . The sabrelite board has 2MB SPI NOR flash but I cannot find "/dev/spidev" entry created in linux kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried steps in these posts but still no "spidev" entry is created.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/302612"&gt;How to enable spidev for all SPI (1-5) for MX6&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/314983"&gt;Can't use spidev on i.MX53.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/301435"&gt;Re: SPI: SPIDEV interface question&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/394060"&gt;/dev/spidev not appearing on iMX6Q despite kernel configuration and modalias="spidev"&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/344410"&gt;Re: spidev&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can access the NOR flash using "sf" command in u-boot. Has anyone successfully able to create "/dev/spidev" entry in linux kernel for sabrelite?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jai Ganesh S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 May 2014 14:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/spidev-on-sabrelite/m-p/312319#M40894</guid>
      <dc:creator>jaiganesh</dc:creator>
      <dc:date>2014-05-08T14:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: spidev on sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/spidev-on-sabrelite/m-p/312320#M40895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the only SPI device on the SABRE Lite (BD-SL-i.MX6) is the SPI-NOR flash, we don't enable userspace SPI in our default configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can enable it using the kernel's "menuconfig" or by adding "CONFIG_SPI_SPIDEV=y" to your kernel configuration, but the SPI-NOR is accessible using the MTD driver, so SPIDEV isn't needed for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on a configuration that will re-purpose the LCD connector (J15) on the SABRE Lite boards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can enable it using the kernel's "menuconfig" or by adding "CONFIG_SPI_SPIDEV=y" to your kernel configuration, but the SPI-NOR is accessible using the MTD driver, so SPIDEV isn't needed for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on customer feedback, we are working on a configuration that will re-purpose the LCD connector (J15) on the SABRE Lite boards as a combination of GPIO and additional SPI channels (ECSPI2/3).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 May 2014 14:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/spidev-on-sabrelite/m-p/312320#M40895</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-05-08T14:17:10Z</dc:date>
    </item>
  </channel>
</rss>