<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can imx6 support for RGB RAW camera? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311378#M40677</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; According to i.MX6 DQ Reference Manual [section 9.2.1.1 (Camera Ports) ],&lt;/P&gt;&lt;P&gt;the IPU&amp;nbsp; supports Raw (Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale &lt;/P&gt;&lt;P&gt;data formats, up to 16 bits per value (component). &lt;/P&gt;&lt;P&gt;&amp;nbsp; I am afraid the IPU does not support conversion Bayer to RGB / YUV in hardware.&lt;/P&gt;&lt;P&gt;Bayer data is a type of generic data from an image sensor. These data should be converted &lt;/P&gt;&lt;P&gt;to the RGB space or YUV space by software (using ARM cores).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 May 2014 07:44:32 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-05-07T07:44:32Z</dc:date>
    <item>
      <title>Can imx6 support for RGB RAW camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311375#M40674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Most high-res cameras only output RGB Raw format data, such as 8MP OV8825, 13MP OV13850,&amp;nbsp; but the RAW RGB format is not support by the IPU of imx6 form the datasheet. The Android BSP of&amp;nbsp; SABRE-SD Board has &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;also&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em; color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; only provided the code of 5MP cameras which output YUV format sensor data. Now, we want to add 8MP or 13MP cameras to our platform, how can we &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;resolve the issue? Do you have any solutions for this issue? &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Rgds&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Dong Xu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 06:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311375#M40674</guid>
      <dc:creator>xudong</dc:creator>
      <dc:date>2014-05-07T06:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6 support for RGB RAW camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311376#M40675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, i.MX6 IPU can support camera r&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;aw format data. Please look at links below&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="331888" data-objecttype="2" href="https://community.freescale.com/message/331888#331888"&gt;https://community.freescale.com/message/331888&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="309833" data-objecttype="2" href="https://community.freescale.com/message/309833#309833"&gt;https://community.freescale.com/message/309833#309833&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="309069" data-objecttype="2" href="https://community.freescale.com/message/309069#309069"&gt;https://community.freescale.com/message/309069#309069&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 07:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311376#M40675</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-07T07:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6 support for RGB RAW camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311377#M40676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;The following is copied from the links you gave me:&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/STRONG&gt; Got some comfirmed information from IC designer, for iMX6, the IPU can't support converting bayer format to RGB/YUV on the fly, it can only use generic mode to receive the CSI input bayer data to memory. The CPD can only be used to convert 10 bits color data to 8 bits.&lt;/EM&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; On iMX5x IPU, there is a module called "ISP" which can be used to handle bayer format data, but it was also not fully verified, so in the iMX5x document, the ISP section had been removed. And on iMX6, that "ISP" module had been removed.&lt;/EM&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp; That means I have to use software to convert the raw RGB to RGB/YUV format for preview and capture, i think it will be very complex and hard to realize. Do you have the converting code or related solutions?&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks! &lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Xu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 07:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311377#M40676</guid>
      <dc:creator>xudong</dc:creator>
      <dc:date>2014-05-07T07:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6 support for RGB RAW camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311378#M40677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; According to i.MX6 DQ Reference Manual [section 9.2.1.1 (Camera Ports) ],&lt;/P&gt;&lt;P&gt;the IPU&amp;nbsp; supports Raw (Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale &lt;/P&gt;&lt;P&gt;data formats, up to 16 bits per value (component). &lt;/P&gt;&lt;P&gt;&amp;nbsp; I am afraid the IPU does not support conversion Bayer to RGB / YUV in hardware.&lt;/P&gt;&lt;P&gt;Bayer data is a type of generic data from an image sensor. These data should be converted &lt;/P&gt;&lt;P&gt;to the RGB space or YUV space by software (using ARM cores).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 07:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311378#M40677</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-05-07T07:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6 support for RGB RAW camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311379#M40678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xu&lt;/P&gt;&lt;P&gt;actually seems there is just confusion in terminology:&lt;/P&gt;&lt;P&gt;format can be "raw" or "RGB" but not both "raw RGB".&lt;/P&gt;&lt;P&gt;I provided links for "r&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;aw format" - actually this may any (even weird) format,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;it can be stored in memory, then in software one can convert it&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;to needed format. Hope this clarify.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue',Helvetica,Arial,'Lucida Grande',sans-serif; font-size: 10pt;"&gt;Regarding "Do you have the converting code or related solutions?" - answer no.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since this is very specific for every non-standard format.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Full list of supported formats is given in &lt;/SPAN&gt;&lt;SPAN&gt;Table 66 "Camera Input Signal Cross &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Reference, Format, and Bits Per Cycle" &lt;/SPAN&gt;i.MX6DQ Datasheet (rev.3, 2/2014)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 12:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6-support-for-RGB-RAW-camera/m-p/311379#M40678</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-07T12:27:16Z</dc:date>
    </item>
  </channel>
</rss>