<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PF0100 question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311266#M40658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks all for great answers!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;I2C is required to program the OTP fuses of the PF0100.&amp;nbsp; When this is done in-circuit, I2C is shared with the CPU.&amp;nbsp; The CPU will not be powered, but I2C will be pulled up to 3.3V through 10K resistors, while NVCC_GPIO is at 0V.&amp;nbsp; Can this damage the I2C pins on the CPU, or will the 10K resistors limit the current sufficiently to be prevent damage?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;Populating and depopulating resistors to program the PF0100 is not a very good solution:&amp;nbsp; it will slow down production, and is mistake-prone.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Apr 2014 16:57:25 GMT</pubDate>
    <dc:creator>jwu</dc:creator>
    <dc:date>2014-04-11T16:57:25Z</dc:date>
    <item>
      <title>PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311261#M40653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;It looks like the programmer supports in-circuit programming for the MMPF0100.&amp;nbsp; Fig. 4 of KTPFPGMEVMEUG shows that I2C and VIN connections on the MMPF0100 are required.&amp;nbsp; Questions / issues:&lt;BR /&gt;&lt;BR /&gt;1.&amp;nbsp; If the CPU is not powered, will pullups on I2C cause problems on the CPU?&lt;BR /&gt;&lt;BR /&gt;2.&amp;nbsp; VDDIO must be connected to VIN, which is not the normal connection on the board.&lt;BR /&gt;&lt;BR /&gt;Do most customers use the socket to program the MMPF0100, and then solder it on the board?&amp;nbsp; This won't allow testing of the configuration, but it will avoid the issues above.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Apr 2014 05:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311261#M40653</guid>
      <dc:creator>jwu</dc:creator>
      <dc:date>2014-04-05T05:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311262#M40654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMPF0100 datasheet, Table 4, Note 5:&lt;BR /&gt;&lt;BR /&gt;"Unused switching regulators should be connected as follow: Pins SWxLX and SWxFB should be unconnected and Pin SWxIN should be connected to VIN with a 0.1uF bypass capacitor."&lt;BR /&gt;&lt;BR /&gt;I can't find a similar note for unused LDOs.&amp;nbsp; Can I leave the outputs of unused LDOs unconnected, or do all LDOs require an output capacitor even if they're not used?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 05:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311262#M40654</guid>
      <dc:creator>jwu</dc:creator>
      <dc:date>2014-04-08T05:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311263#M40655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the I2C and VIN connections should be designed as optional circuit, they do affect the CPU. &lt;/P&gt;&lt;P&gt;when you program pfuse, you connect the I2C and VIN for pfuse. when you finish the program, you should remove these optional parts (resisters....)&lt;/P&gt;&lt;P&gt;so the the I2C and VIN are only for program and should be optional with resisters. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 08:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311263#M40655</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-04-08T08:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311264#M40656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi, John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for LDO, I think you can refer to SW, add 0.1uF on the input and leave the output float.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 08:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311264#M40656</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-04-08T08:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311265#M40657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717 &lt;/P&gt;&lt;P&gt;(Schematic Guidelines for the MMPF0100).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf"&gt;http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Apr 2014 09:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311265#M40657</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-04-08T09:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311266#M40658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks all for great answers!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;I2C is required to program the OTP fuses of the PF0100.&amp;nbsp; When this is done in-circuit, I2C is shared with the CPU.&amp;nbsp; The CPU will not be powered, but I2C will be pulled up to 3.3V through 10K resistors, while NVCC_GPIO is at 0V.&amp;nbsp; Can this damage the I2C pins on the CPU, or will the 10K resistors limit the current sufficiently to be prevent damage?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;Populating and depopulating resistors to program the PF0100 is not a very good solution:&amp;nbsp; it will slow down production, and is mistake-prone.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Apr 2014 16:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311266#M40658</guid>
      <dc:creator>jwu</dc:creator>
      <dc:date>2014-04-11T16:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311267#M40659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 12pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;3.&amp;nbsp; Section 4.9.1 of IMX6SDLIEC:&amp;nbsp; &lt;EM&gt;SRC_POR_B rise and fall times must be 5ns or less.&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;POR_B has an internal 100K pullup, and the Sabre design does not have any additional pullups.&amp;nbsp; POR_B is driven by an open-drain output on the PMIC.&amp;nbsp; Even with a board and pin capacitance as low as 10pF, the rise time will be 5RC = 5us = 5000ns.&lt;BR /&gt;&lt;BR /&gt;4. The Sabre design uses a pushbutton with a 0.1uF capacitor on the PF0100's PWRON, as a means of resetting the CPU.&amp;nbsp; Is this the best way to do it?&amp;nbsp; It will in effect cycle power, as all power supplies on the PMIC will be turned off and then on again.&amp;nbsp; Why not use POR_B to reset the CPU?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Apr 2014 22:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311267#M40659</guid>
      <dc:creator>jwu</dc:creator>
      <dc:date>2014-04-13T22:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311268#M40660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Weisong&lt;/P&gt;&lt;P&gt;Could you keep following the thread so that we can close the customer's issues?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jun 2014 02:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311268#M40660</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-06-20T02:49:07Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311269#M40661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Weisong&lt;/P&gt;&lt;P&gt;Could you finish the following-up of this customer's issue, or need help from others?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 08:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311269#M40661</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-06-30T08:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311270#M40662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Alfred1z"&gt;Alfred1z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Please see if you are able to help this customer's request. If you need help from others please let me know.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 05:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311270#M40662</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-07-15T05:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311271#M40663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;from my understanding, this optional circuit is just for test or debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for mass production, you can ask FSL programme the chip for you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 06:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311271#M40663</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-07-15T06:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311272#M40664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe the "5ns" is a typo in document, I don;t see this information in latest imx6QD document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jul 2014 06:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311272#M40664</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-07-15T06:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311273#M40665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should we close the issue since Weisong replied you already?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 07:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311273#M40665</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-07-30T07:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311274#M40666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 07:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/311274#M40666</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-08-18T07:24:47Z</dc:date>
    </item>
  </channel>
</rss>