<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx6 uart tx in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-uart-tx/m-p/311036#M40628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the UART5 on the i.mx6 on our board (Yocto project).&lt;/P&gt;&lt;P&gt;I'm using minicom as a terminal and it works fine to receive data, but I can't see any activity on the TX pin (CSI0_DAT14).&lt;/P&gt;&lt;P&gt;I have also tried to write small test code to write on the UART, but the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone who has a suggestion what could be wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I need to think of when setting up the UART in my device tree file?&lt;/P&gt;&lt;P&gt;My current settings:&lt;/P&gt;&lt;P&gt;uart5: serial@021f4000 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; compatible = "fsl,imx6q-uart", "fsl,imx21-uart";&lt;/P&gt;&lt;P&gt;&amp;nbsp; reg = &amp;lt;0x021f4000 0x4000&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; interrupts = &amp;lt;0 30 0x04&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; clocks = &amp;lt;&amp;amp;clks 160&amp;gt;, &amp;lt;&amp;amp;clks 161&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; clock-names = "ipg", "per";&lt;/P&gt;&lt;P&gt;&amp;nbsp; dmas = &amp;lt;&amp;amp;sdma 33 4 0&amp;gt;, &amp;lt;&amp;amp;sdma 34 4 0&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; dma-names = "rx", "tx";&lt;/P&gt;&lt;P&gt;&amp;nbsp; status = "disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uart5 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl_uart5_1: uart5grp-1 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; fsl,pins = &amp;lt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; MX6QDL_PAD_CSI0_DAT15__UART5_RX_DATA 0x1b0b1&lt;/P&gt;&lt;P&gt;&amp;nbsp; MX6QDL_PAD_CSI0_DAT14__UART5_TX_DATA 0x1b0b1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&amp;amp;uart5 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl-names = "default";&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart5_1&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 May 2014 16:38:56 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2014-05-06T16:38:56Z</dc:date>
    <item>
      <title>i.mx6 uart tx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-uart-tx/m-p/311036#M40628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the UART5 on the i.mx6 on our board (Yocto project).&lt;/P&gt;&lt;P&gt;I'm using minicom as a terminal and it works fine to receive data, but I can't see any activity on the TX pin (CSI0_DAT14).&lt;/P&gt;&lt;P&gt;I have also tried to write small test code to write on the UART, but the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone who has a suggestion what could be wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I need to think of when setting up the UART in my device tree file?&lt;/P&gt;&lt;P&gt;My current settings:&lt;/P&gt;&lt;P&gt;uart5: serial@021f4000 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; compatible = "fsl,imx6q-uart", "fsl,imx21-uart";&lt;/P&gt;&lt;P&gt;&amp;nbsp; reg = &amp;lt;0x021f4000 0x4000&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; interrupts = &amp;lt;0 30 0x04&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; clocks = &amp;lt;&amp;amp;clks 160&amp;gt;, &amp;lt;&amp;amp;clks 161&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; clock-names = "ipg", "per";&lt;/P&gt;&lt;P&gt;&amp;nbsp; dmas = &amp;lt;&amp;amp;sdma 33 4 0&amp;gt;, &amp;lt;&amp;amp;sdma 34 4 0&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; dma-names = "rx", "tx";&lt;/P&gt;&lt;P&gt;&amp;nbsp; status = "disabled";&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uart5 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl_uart5_1: uart5grp-1 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; fsl,pins = &amp;lt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; MX6QDL_PAD_CSI0_DAT15__UART5_RX_DATA 0x1b0b1&lt;/P&gt;&lt;P&gt;&amp;nbsp; MX6QDL_PAD_CSI0_DAT14__UART5_TX_DATA 0x1b0b1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&amp;amp;uart5 {&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl-names = "default";&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart5_1&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 16:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-uart-tx/m-p/311036#M40628</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-05-06T16:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 uart tx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-uart-tx/m-p/311037#M40629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Seems like I had HW flow control enabled.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 17:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-uart-tx/m-p/311037#M40629</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-05-06T17:11:21Z</dc:date>
    </item>
  </channel>
</rss>