<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: DDR3 clock domain</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-clock-domain/m-p/310949#M40613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi alesandro, &lt;/P&gt;&lt;P&gt;on MCIMX6Q-SMART DEVICE BOARD, pag. 4&lt;/P&gt;&lt;P&gt;all 4 memory chip, all DDR3 are connected to DRAM_CS0,&lt;/P&gt;&lt;P&gt;so DRAM_SDCKE1,DRAM_SDODT1 are not used (they are used&lt;/P&gt;&lt;P&gt;with&amp;nbsp; DRAM_CS0). However DRAM_SDCLK0,DRAM_SDCLK1 is the&lt;/P&gt;&lt;P&gt;same signal (duplicates each other).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 May 2014 03:34:26 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-05-07T03:34:26Z</dc:date>
    <item>
      <title>DDR3 clock domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-clock-domain/m-p/310948#M40612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've been working on the hardware of a board with a 4core i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 4 memory chip, all DDR3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the reference design (MCIMX6Q-SMART DEVICE BOARD, pag. 4), I see that:&lt;/P&gt;&lt;P&gt;- two DDR3 modules are connected to &lt;EM&gt;&lt;STRONG&gt;DRAM_SDCLK0&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;- two DDR3 modules are connected to &lt;EM&gt;&lt;STRONG&gt;DRAM_SDCLK1&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The clock enable used is &lt;EM&gt;&lt;STRONG&gt;DRAM_SDCKE0&lt;/STRONG&gt;&lt;/EM&gt; while &lt;EM&gt;&lt;STRONG&gt;DRAM_SDCKE1&lt;/STRONG&gt;&lt;/EM&gt; is unconnected.&lt;/P&gt;&lt;P&gt;Also &lt;EM&gt;&lt;STRONG&gt;DRAM_SDODT0&lt;/STRONG&gt;&lt;/EM&gt; controls the on-die termination of all the four modules while &lt;EM&gt;&lt;STRONG&gt;DRAM_SDODT1&lt;/STRONG&gt;&lt;/EM&gt; is unconnected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Alessandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 13:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-clock-domain/m-p/310948#M40612</guid>
      <dc:creator>pscz</dc:creator>
      <dc:date>2014-05-06T13:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 clock domain</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR3-clock-domain/m-p/310949#M40613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi alesandro, &lt;/P&gt;&lt;P&gt;on MCIMX6Q-SMART DEVICE BOARD, pag. 4&lt;/P&gt;&lt;P&gt;all 4 memory chip, all DDR3 are connected to DRAM_CS0,&lt;/P&gt;&lt;P&gt;so DRAM_SDCKE1,DRAM_SDODT1 are not used (they are used&lt;/P&gt;&lt;P&gt;with&amp;nbsp; DRAM_CS0). However DRAM_SDCLK0,DRAM_SDCLK1 is the&lt;/P&gt;&lt;P&gt;same signal (duplicates each other).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 03:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR3-clock-domain/m-p/310949#M40613</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-07T03:34:26Z</dc:date>
    </item>
  </channel>
</rss>