<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Parallel LCD issue on Android in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-LCD-issue-on-Android/m-p/310805#M40567</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following U-boot variable is used with the LCD :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB24&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an example :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB24 ip=none'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="309048" data-objecttype="1" href="https://community.freescale.com/thread/309048"&gt;https://community.freescale.com/thread/309048&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 May 2014 05:05:39 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-05-07T05:05:39Z</dc:date>
    <item>
      <title>Parallel LCD issue on Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-LCD-issue-on-Android/m-p/310804#M40566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using a 24 bit parallel LCD(800x480) with sabresd board. I am using the android code provided by freescale. Here is the kernel commandline argument provided to activate the parallel display -&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp; &lt;/STRONG&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;I am using the driver drivers/video/mxc/mxc_lcdif.c for the LCD display and confirmed that the following parameters in driver is confirming the display specifications -&lt;/P&gt;&lt;P&gt;static struct fb_videomode lcdif_modedb[] = {&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;/* 800x480 @ 57 Hz , pixel clk @ 27MHz */&lt;/P&gt;&lt;P&gt;"CLAA-WVGA", 57, 480,800, 37037, 40, 60, 10, 10, 20, 10,&lt;/P&gt;&lt;P&gt;FB_SYNC_CLK_LAT_FALL,&lt;/P&gt;&lt;P&gt;FB_VMODE_NONINTERLACED,&lt;/P&gt;&lt;P&gt;0,}&lt;/P&gt;&lt;P&gt;The problem is that the display is comming but it is bit distorted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 09:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Parallel-LCD-issue-on-Android/m-p/310804#M40566</guid>
      <dc:creator>benoysaha</dc:creator>
      <dc:date>2014-05-06T09:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: Parallel LCD issue on Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Parallel-LCD-issue-on-Android/m-p/310805#M40567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following U-boot variable is used with the LCD :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB24&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an example :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB24 ip=none'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="309048" data-objecttype="1" href="https://community.freescale.com/thread/309048"&gt;https://community.freescale.com/thread/309048&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 05:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Parallel-LCD-issue-on-Android/m-p/310805#M40567</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-05-07T05:05:39Z</dc:date>
    </item>
  </channel>
</rss>