<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Mfgtool2 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool2/m-p/310531#M40505</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yufeng,&lt;/P&gt;&lt;P&gt;Under the Win7, the device works and can be detected. Here I recommend you to have a try another USB port. Maybe the port you are using are old.&lt;/P&gt;&lt;P&gt;Hope this can help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jun 2014 03:09:17 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2014-06-03T03:09:17Z</dc:date>
    <item>
      <title>Mfgtool2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool2/m-p/310530#M40504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;通过Mfgtool2工具加载boot和内核，WinXP下正常，Win7无法识别到设备。请问是什么原因。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;谢谢！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 03:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool2/m-p/310530#M40504</guid>
      <dc:creator>yufengzhao</dc:creator>
      <dc:date>2014-06-03T03:00:15Z</dc:date>
    </item>
    <item>
      <title>Re: Mfgtool2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mfgtool2/m-p/310531#M40505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi yufeng,&lt;/P&gt;&lt;P&gt;Under the Win7, the device works and can be detected. Here I recommend you to have a try another USB port. Maybe the port you are using are old.&lt;/P&gt;&lt;P&gt;Hope this can help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Dan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 03:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mfgtool2/m-p/310531#M40505</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2014-06-03T03:09:17Z</dc:date>
    </item>
  </channel>
</rss>