<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SDK - Enabling interrupts under u-boot control</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Enabling-interrupts-under-u-boot-control/m-p/310112#M40350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;the current platform SDK (version 1.1.0) provides some examples which are using interrupts.&lt;/P&gt;&lt;P&gt;The examples which are not using interrupts can be successfully loaded and started with u-boot commands.&lt;BR /&gt;If you try to to start an example (under u-boot control) which uses interrupts the system will hang.&lt;/P&gt;&lt;P&gt;Attached you will find a patch series which solves this issue on my side. (the patch is for RFC and contains only one example: epit)&lt;/P&gt;&lt;P&gt;BTW, for tests I use a Sabre Lite development board (i.MX6 quad core).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0002-SDK-fix-linker-script-for-VBAR-support.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0003-SDK-epit-test-fix-interrupt-support-by-using-VBAR.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0001-Cortex-A9-add-get-set-_vbar-helper-functions.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jun 2014 18:30:10 GMT</pubDate>
    <dc:creator>dancer</dc:creator>
    <dc:date>2014-06-02T18:30:10Z</dc:date>
    <item>
      <title>SDK - Enabling interrupts under u-boot control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Enabling-interrupts-under-u-boot-control/m-p/310112#M40350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;the current platform SDK (version 1.1.0) provides some examples which are using interrupts.&lt;/P&gt;&lt;P&gt;The examples which are not using interrupts can be successfully loaded and started with u-boot commands.&lt;BR /&gt;If you try to to start an example (under u-boot control) which uses interrupts the system will hang.&lt;/P&gt;&lt;P&gt;Attached you will find a patch series which solves this issue on my side. (the patch is for RFC and contains only one example: epit)&lt;/P&gt;&lt;P&gt;BTW, for tests I use a Sabre Lite development board (i.MX6 quad core).&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0002-SDK-fix-linker-script-for-VBAR-support.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0003-SDK-epit-test-fix-interrupt-support-by-using-VBAR.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337071"&gt;0001-Cortex-A9-add-get-set-_vbar-helper-functions.patch.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jun 2014 18:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-Enabling-interrupts-under-u-boot-control/m-p/310112#M40350</guid>
      <dc:creator>dancer</dc:creator>
      <dc:date>2014-06-02T18:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: SDK - Enabling interrupts under u-boot control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDK-Enabling-interrupts-under-u-boot-control/m-p/310113#M40351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ralf&lt;/P&gt;&lt;P&gt;thanks for sharing codes and experience.&lt;/P&gt;&lt;P&gt;I think is will be useful for board bring-up purposes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 05:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDK-Enabling-interrupts-under-u-boot-control/m-p/310113#M40351</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-03T05:55:47Z</dc:date>
    </item>
  </channel>
</rss>