<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Reading the PMIC values in  Kernel Command Line in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reading-the-PMIC-values-in-Kernel-Command-Line/m-p/310006#M40341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please excuse if it is not a very intelligent question,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a beginner in linux kernel and application development,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6q board which has a MMPF10010 PMIC chip .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to see the corresponding voltages when i boot the kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;print_constraints: SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1375 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1375 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW4: 800 &amp;lt;--&amp;gt; 3950 mV at 3150 mV&lt;/P&gt;&lt;P&gt;print_constraints: SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV&lt;/P&gt;&lt;P&gt;print_constraints: VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VREFDDR: at 750 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i am not able to figure out how i can print these values after my processor is booted in the kernel command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any command using which i can do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Apr 2014 12:47:28 GMT</pubDate>
    <dc:creator>nishad_kamdar</dc:creator>
    <dc:date>2014-04-03T12:47:28Z</dc:date>
    <item>
      <title>Reading the PMIC values in  Kernel Command Line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-the-PMIC-values-in-Kernel-Command-Line/m-p/310006#M40341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please excuse if it is not a very intelligent question,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a beginner in linux kernel and application development,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6q board which has a MMPF10010 PMIC chip .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to see the corresponding voltages when i boot the kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;print_constraints: SW1A: 300 &amp;lt;--&amp;gt; 1875 mV at 1375 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW1B: 300 &amp;lt;--&amp;gt; 1875 mV at 300 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW1C: 300 &amp;lt;--&amp;gt; 1875 mV at 1375 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: SW4: 800 &amp;lt;--&amp;gt; 3950 mV at 3150 mV&lt;/P&gt;&lt;P&gt;print_constraints: SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV&lt;/P&gt;&lt;P&gt;print_constraints: VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VREFDDR: at 750 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN1: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN2: 800 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2500 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV&lt;/P&gt;&lt;P&gt;print_constraints: VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i am not able to figure out how i can print these values after my processor is booted in the kernel command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any command using which i can do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 12:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-the-PMIC-values-in-Kernel-Command-Line/m-p/310006#M40341</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-04-03T12:47:28Z</dc:date>
    </item>
  </channel>
</rss>