<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Accessing Parallel Nor flash in Kernel Command Line in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-Parallel-Nor-flash-in-Kernel-Command-Line/m-p/309965#M40340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may use "memtool" utility in /unit/tests directory.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Apr 2014 07:21:38 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-04-04T07:21:38Z</dc:date>
    <item>
      <title>Accessing Parallel Nor flash in Kernel Command Line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-Parallel-Nor-flash-in-Kernel-Command-Line/m-p/309964#M40339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6q board in which i have a parallel nor flash connected to the Processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to read and write to it in u-boot using the "md" command however i am not able to do it in &lt;/P&gt;&lt;P&gt;Kernel command line after my linux boots.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me how i can read and write to the Nor flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 12:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-Parallel-Nor-flash-in-Kernel-Command-Line/m-p/309964#M40339</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-04-03T12:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing Parallel Nor flash in Kernel Command Line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-Parallel-Nor-flash-in-Kernel-Command-Line/m-p/309965#M40340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may use "memtool" utility in /unit/tests directory.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 07:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-Parallel-Nor-flash-in-Kernel-Command-Line/m-p/309965#M40340</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-04-04T07:21:38Z</dc:date>
    </item>
  </channel>
</rss>