<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: how to install multiple BSPs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163917#M4028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You for the replay.&lt;/P&gt;&lt;P&gt;Do you remove all previously installed packages in /opt/freescale/pkgs when you install a new BSP (as stated below)?&lt;/P&gt;&lt;P&gt;If so these files are used only during the ltib installation .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX53_START_Linux_BSP_UserGuide.pdf :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Installing and Building LTIB&lt;/P&gt;&lt;P&gt;To install and build LTIB, follow the steps below:&lt;/P&gt;&lt;P&gt; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Remove all previously-installed packages in /opt/freescale/pkgs/.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Nov 2012 18:04:56 GMT</pubDate>
    <dc:creator>yektaayduk</dc:creator>
    <dc:date>2012-11-06T18:04:56Z</dc:date>
    <item>
      <title>how to install multiple BSPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163915#M4026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Currently I'm using the BSP (1)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX536&amp;amp;nodeId=018rH3ZrDR988D&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.35_11_09_ER_SOURCE&lt;/A&gt;&amp;nbsp; for imx53 .&lt;/P&gt;&lt;P&gt;I had a previous installtion for imx25&amp;nbsp; BSP(2)&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX258&amp;amp;nodeId=018rH3ZrDR6B45&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L2.6.31_09.12.00_SDK_SOURCE&amp;nbsp; &lt;/A&gt;,but I removed it because in the&lt;/P&gt;&lt;P&gt;ltib user guide for imx53&amp;nbsp; it says : remove any previous installation&amp;nbsp; packages under /opt/freescale/pkgs .&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have an imx25 -3 stack board and want to boot the board from SDcard.&lt;/P&gt;&lt;P&gt;Using this BSP(1) I can compile uboot for imx25 ,but I want to build a rootfs.ext3 for imx25 .&lt;/P&gt;&lt;P&gt;The ltib BSP(1) has only board selections for imx 5x family for kernel compilation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is ,(how) can we install multiple&amp;nbsp; i.mx BSPs and use them ?&lt;/P&gt;&lt;P&gt;Is there any other BSP which covers all i.mx processors?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Nov 2012 12:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163915#M4026</guid>
      <dc:creator>yektaayduk</dc:creator>
      <dc:date>2012-11-04T12:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: how to install multiple BSPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163916#M4027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no BSP to cover ALL imx processors. Please use 11.09 for imx53 and 09.12 for imx25.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since imx27 i've been installing every new BSP to my home folder. I think latest BSP I installed in my PC was 11.09 for imx53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had no big problem for doing this. Any LTIB problem I faced was resolved someway.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2012 16:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163916#M4027</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-11-06T16:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: how to install multiple BSPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163917#M4028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You for the replay.&lt;/P&gt;&lt;P&gt;Do you remove all previously installed packages in /opt/freescale/pkgs when you install a new BSP (as stated below)?&lt;/P&gt;&lt;P&gt;If so these files are used only during the ltib installation .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX53_START_Linux_BSP_UserGuide.pdf :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Installing and Building LTIB&lt;/P&gt;&lt;P&gt;To install and build LTIB, follow the steps below:&lt;/P&gt;&lt;P&gt; ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Remove all previously-installed packages in /opt/freescale/pkgs/.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2012 18:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163917#M4028</guid>
      <dc:creator>yektaayduk</dc:creator>
      <dc:date>2012-11-06T18:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: how to install multiple BSPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163918#M4029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have never cared about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, if there is such warning, maybe someone had have some mistake in the past. Or maybe, because you end up with a lot of carbage in /opr/freescale/pkgs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have never had problem with it, but I always used Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try to change the ltib file (file is called ltib, it's a script you can edit) in order to have a different /opt/freescale/pkgs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a lot of files inside /opt/freescale/pkgs. If bsp 11.09 uses (i.e) alsa-1.10 and bsp uses alsa-1.9 you will end up with both, but your ltib will only take that one it needs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2012 18:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-install-multiple-BSPs/m-p/163918#M4029</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2012-11-06T18:54:34Z</dc:date>
    </item>
  </channel>
</rss>