<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Nitrogen6X Lilliput in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309219#M40066</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a 7" Lilliput 669B LCD with a Boundary devices Nitrogen6X and the Yocto build.&amp;nbsp; I would like to run the HDMI at 800x480 and force this resolution.&amp;nbsp; I tried to set it but it just reverts back to the 720x480 resolution.&amp;nbsp; Has anyone gotten a non-standard HDMI mode to work with this image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I would like to use the touchscreen on my board which is a capacitive touch Atmel maXTouch.&amp;nbsp; It is listed in the USB devices but tslib gets 0 for all the press corrdinates.&amp;nbsp; Has anyone used this touchscreen with the Nitrogen6x yocto build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Apr 2014 00:10:25 GMT</pubDate>
    <dc:creator>BrianEdmond</dc:creator>
    <dc:date>2014-04-03T00:10:25Z</dc:date>
    <item>
      <title>Nitrogen6X Lilliput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309219#M40066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a 7" Lilliput 669B LCD with a Boundary devices Nitrogen6X and the Yocto build.&amp;nbsp; I would like to run the HDMI at 800x480 and force this resolution.&amp;nbsp; I tried to set it but it just reverts back to the 720x480 resolution.&amp;nbsp; Has anyone gotten a non-standard HDMI mode to work with this image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I would like to use the touchscreen on my board which is a capacitive touch Atmel maXTouch.&amp;nbsp; It is listed in the USB devices but tslib gets 0 for all the press corrdinates.&amp;nbsp; Has anyone used this touchscreen with the Nitrogen6x yocto build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 00:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309219#M40066</guid>
      <dc:creator>BrianEdmond</dc:creator>
      <dc:date>2014-04-03T00:10:25Z</dc:date>
    </item>
    <item>
      <title>Re: Nitrogen6X Lilliput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309220#M40067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a long, sordid story, but I'll try to summarize:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The default kernel from Freescale only supports "CEA" modes (common resolutions for consumer electronics) because there are clocking issues within the kernel. In essence, there are only a handful of divisors of the video clock to get proper audio output over HDMI.&lt;/LI&gt;&lt;LI&gt;We naively bypassed this check, then started hearing about troubles with audio,&lt;/LI&gt;&lt;LI&gt;Then we imposed a requirement for a kernel parameter "mxc_hdmi.only_cea=0" and made the default =1&lt;/LI&gt;&lt;LI&gt;You can over-ride this by setting "allow_noncea" to 1 in U-Boot, but you will get screwed up audio playback over HDMI.&lt;BR /&gt;&lt;BR /&gt;&lt;PRE&gt;U-Boot &amp;gt; setenv allow_noncea 1
U-Boot &amp;gt; saveenv &amp;amp;&amp;amp; boot
&lt;/PRE&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can read more about it here (with references to the sources):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://boundarydevices.com/hdmi/" rel="nofollow noopener noreferrer" title="http://boundarydevices.com/hdmi/" target="_blank"&gt;http://boundarydevices.com/hdmi/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The boot script fragment is here:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://github.com/boundarydevices/u-boot-imx6/blob/production/board/boundary/nitrogen6x/6x_bootscript.txt#L114" rel="nofollow noopener noreferrer" title="https://github.com/boundarydevices/u-boot-imx6/blob/production/board/boundary/nitrogen6x/6x_bootscript.txt#L114" target="_blank"&gt;u-boot-imx6/board/boundary/nitrogen6x/6x_bootscript.txt at production · boundarydevices/u-boot-imx6 · GitHub&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 00:57:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309220#M40067</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-04-03T00:57:14Z</dc:date>
    </item>
    <item>
      <title>Re: Nitrogen6X Lilliput</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309221#M40068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I forgot to answer your question about the Atmel MaXtouch USB driver...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We haven't seen one of these, so there's currently no support in the kernel tree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We do have support for an I2C version of a MaXtouch controller, though it's not enabled in our standard configurations.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Apr 2014 00:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6X-Lilliput/m-p/309221#M40068</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-04-03T00:59:21Z</dc:date>
    </item>
  </channel>
</rss>