<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic hard-float in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/hard-float/m-p/309185#M40064</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if Yocto is supporting hard-floating for i.MX6?&lt;/P&gt;&lt;P&gt;Or do I need to include this part when I compile a specific application, node.Js in our case?&lt;/P&gt;&lt;P&gt;If so, how do I change the compile to use hard-float instead?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Apr 2014 20:34:00 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2014-04-02T20:34:00Z</dc:date>
    <item>
      <title>hard-float</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hard-float/m-p/309185#M40064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if Yocto is supporting hard-floating for i.MX6?&lt;/P&gt;&lt;P&gt;Or do I need to include this part when I compile a specific application, node.Js in our case?&lt;/P&gt;&lt;P&gt;If so, how do I change the compile to use hard-float instead?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 20:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hard-float/m-p/309185#M40064</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-04-02T20:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: hard-float</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/hard-float/m-p/309186#M40065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It does support and by default it is HF. Check the DEFAULTTUNE  variable in case you want to change it to SF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 22:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/hard-float/m-p/309186#M40065</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2014-04-02T22:06:04Z</dc:date>
    </item>
  </channel>
</rss>