<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can't capture data from adv7611 with CSI0 on MX6Q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307850#M39764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working with two sensor inputs on i.mx6q/linux platform.&lt;/P&gt;&lt;P&gt;One is adv7180 in PAL mode connected to CSI1 IPU2.&lt;/P&gt;&lt;P&gt;It works fairly well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other one is adv7611 connected to CSI0 IPU1.&lt;/P&gt;&lt;P&gt;We cannot get any data from CSI0 port by now.&lt;/P&gt;&lt;P&gt;The 'mxc_v4l2_capture.out' application gives &lt;/P&gt;&lt;P&gt;'ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0'.&lt;/P&gt;&lt;P&gt;It means that no data arrive CSI0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have setting adv7611 to work in free run mode, &lt;/P&gt;&lt;P&gt;which produces a 8Bit BT656 bit stream for 576i video mode.&lt;/P&gt;&lt;P&gt;The output Vsync, Hsync, Pixclk signals seem good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the register settings for CSI0 is basically the same as the settings of CSI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 May 2014 06:13:32 GMT</pubDate>
    <dc:creator>RobbieJiang</dc:creator>
    <dc:date>2014-05-29T06:13:32Z</dc:date>
    <item>
      <title>Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307850#M39764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working with two sensor inputs on i.mx6q/linux platform.&lt;/P&gt;&lt;P&gt;One is adv7180 in PAL mode connected to CSI1 IPU2.&lt;/P&gt;&lt;P&gt;It works fairly well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other one is adv7611 connected to CSI0 IPU1.&lt;/P&gt;&lt;P&gt;We cannot get any data from CSI0 port by now.&lt;/P&gt;&lt;P&gt;The 'mxc_v4l2_capture.out' application gives &lt;/P&gt;&lt;P&gt;'ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0'.&lt;/P&gt;&lt;P&gt;It means that no data arrive CSI0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have setting adv7611 to work in free run mode, &lt;/P&gt;&lt;P&gt;which produces a 8Bit BT656 bit stream for 576i video mode.&lt;/P&gt;&lt;P&gt;The output Vsync, Hsync, Pixclk signals seem good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the register settings for CSI0 is basically the same as the settings of CSI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 06:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307850#M39764</guid>
      <dc:creator>RobbieJiang</dc:creator>
      <dc:date>2014-05-29T06:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307851#M39765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robbie,&lt;/P&gt;&lt;P&gt;had you checked link below&lt;/P&gt;&lt;P&gt;(problem was with the Data Enable)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/343035"&gt;IPU2 for CSI parallel camera&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 May 2014 10:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307851#M39765</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-30T10:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307852#M39766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Robbie-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you able to get the ADV7611 input running?&amp;nbsp; I seem to be having the same problem as you with the DE pin set correctly in the DTB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you mind sharing your driver file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Allan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 17:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307852#M39766</guid>
      <dc:creator>allanmatthew</dc:creator>
      <dc:date>2014-08-22T17:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307853#M39767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Allan.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My 7611 works in 12bit BT.1120 mode.&lt;/P&gt;&lt;P&gt;First ensure that the hardware connection between 7611 and MX6 is compatible&lt;/P&gt;&lt;P&gt;with the way specified in MX6Q datasheet.&lt;/P&gt;&lt;P&gt;Also you need to set those IO pins in correct work mode by setting PAD_CTL registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the CSI interface must be set in the same mode as 7611's output.&lt;/P&gt;&lt;P&gt;Otherwise MX6 can not understand incoming data, even if there are video data arriving at CSI interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robbie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 13:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307853#M39767</guid>
      <dc:creator>RobbieJiang</dc:creator>
      <dc:date>2014-08-25T13:16:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307854#M39768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robbie-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp; My HSYNC/VSYNC/DE/PIXCLK signals all appear good.&amp;nbsp; All are active-high, there are blanking periods and the timing looks correct.&amp;nbsp; Were you able to get it working in BT656?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you don't mind, are you using any of the sync pins?&amp;nbsp; What does your ioctl_g_ifparm() function look like?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Allan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 01:21:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307854#M39768</guid>
      <dc:creator>allanmatthew</dc:creator>
      <dc:date>2014-08-26T01:21:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307855#M39769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/RobbieJiang"&gt;RobbieJiang&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please describe how did you connect ADV7611 in 12-bit mode to I.MX6?&lt;/P&gt;&lt;P&gt;I've checked Table 62. Camera Input Signal Cross Reference in "i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet (REV 4)", but there is no mention of 12-bit mode at all.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 16:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307855#M39769</guid>
      <dc:creator>clx</dc:creator>
      <dc:date>2015-08-20T16:07:06Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307856#M39770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did not use 12-bit input for our ADV7611, but 16-bit at last.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For 12-bit CSI input, it is still possible, by properly configuring SENS_CONF registers. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Sep 2015 13:56:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307856#M39770</guid>
      <dc:creator>RobbieJiang</dc:creator>
      <dc:date>2015-09-13T13:56:15Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307857#M39771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer!&lt;/P&gt;&lt;P&gt;One more question, did you connect it like this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CSIx_DAT2&amp;nbsp;&amp;nbsp; ~ CSIx_DAT9&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;----&amp;gt;&amp;nbsp; ADV7611_P0 ~ ADV7611_P7 &lt;/P&gt;&lt;P&gt;CSIx_DAT12 ~ CSIx_DAT19&amp;nbsp;&amp;nbsp; &amp;lt;----&amp;gt;&amp;nbsp; ADV7611_P8 ~ ADV7611_P15 &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Sep 2015 09:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307857#M39771</guid>
      <dc:creator>clx</dc:creator>
      <dc:date>2015-09-14T09:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can't capture data from adv7611 with CSI0 on MX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307858#M39772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, exactly.&lt;/P&gt;&lt;P&gt;​&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Sep 2015 06:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-capture-data-from-adv7611-with-CSI0-on-MX6Q/m-p/307858#M39772</guid>
      <dc:creator>RobbieJiang</dc:creator>
      <dc:date>2015-09-15T06:50:56Z</dc:date>
    </item>
  </channel>
</rss>