<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MX6 UART3 (ttymxc2) Rx not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6-UART3-ttymxc2-Rx-not-working/m-p/307413#M39686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved. Caused by HW &lt;SPAN class="st"&gt;solder empty.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;HW wire connection should be:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;USB TTL RXD --&amp;gt; R194&amp;nbsp; (imx6 UART3&amp;nbsp; TX)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;USB TTL TXD --&amp;gt; R192&amp;nbsp;&amp;nbsp; &lt;SPAN class="st"&gt;(imx6 UART3&amp;nbsp; RX)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;then &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;disable GPS configuration in init.rc&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;UART3 TX/RX works.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Apr 2014 10:57:10 GMT</pubDate>
    <dc:creator>jimmysu</dc:creator>
    <dc:date>2014-04-01T10:57:10Z</dc:date>
    <item>
      <title>MX6 UART3 (ttymxc2) Rx not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-UART3-ttymxc2-Rx-not-working/m-p/307412#M39685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr./Mrs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was trying to connect the imx6q-sabresd board to a rs232 devices via uart3.&lt;/P&gt;&lt;P&gt;The BSP version is L3.0.35_4.1.0_130816 with Android 4.3.&lt;/P&gt;&lt;P&gt;Now, I can test uart3 by typing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; echo "test" &amp;gt; /dev/ttymxc2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Its working.&lt;/P&gt;&lt;P&gt;But it can't receive data when I test it by using serial port console app.&lt;/P&gt;&lt;P&gt;Is there anyone can help on this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 03:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-UART3-ttymxc2-Rx-not-working/m-p/307412#M39685</guid>
      <dc:creator>jimmysu</dc:creator>
      <dc:date>2014-04-01T03:38:40Z</dc:date>
    </item>
    <item>
      <title>Re: MX6 UART3 (ttymxc2) Rx not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6-UART3-ttymxc2-Rx-not-working/m-p/307413#M39686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved. Caused by HW &lt;SPAN class="st"&gt;solder empty.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;HW wire connection should be:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;USB TTL RXD --&amp;gt; R194&amp;nbsp; (imx6 UART3&amp;nbsp; TX)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;USB TTL TXD --&amp;gt; R192&amp;nbsp;&amp;nbsp; &lt;SPAN class="st"&gt;(imx6 UART3&amp;nbsp; RX)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;then &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;disable GPS configuration in init.rc&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="st"&gt;&lt;SPAN class="st"&gt;UART3 TX/RX works.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 10:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6-UART3-ttymxc2-Rx-not-working/m-p/307413#M39686</guid>
      <dc:creator>jimmysu</dc:creator>
      <dc:date>2014-04-01T10:57:10Z</dc:date>
    </item>
  </channel>
</rss>