<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Re: something  wrong with 1080P on IMX535</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307286#M39671</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi chipexpert：&lt;/P&gt;&lt;P&gt;&amp;nbsp; we have requrement 1080P for&amp;nbsp; customer .&lt;/P&gt;&lt;P&gt;&amp;nbsp; I want to know why I can't measure the CLK of LVDS pin.&lt;/P&gt;&lt;P&gt; Please see attached file. Is there something wrong with sch? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 May 2014 02:00:59 GMT</pubDate>
    <dc:creator>leeo</dc:creator>
    <dc:date>2014-05-05T02:00:59Z</dc:date>
    <item>
      <title>something  wrong with 1080P on IMX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307284#M39669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have heared that many people say lvds can't output 1080P, when I try to&amp;nbsp; check source code ,&lt;/P&gt;&lt;P&gt;If i set the mode is "Spilt",&lt;BR /&gt;the code will set the&amp;nbsp; pixclk is 2*455/7=120M pixclk/s,&lt;/P&gt;&lt;P&gt;check as double rate ,it will be 240M, It will be larger than the width 1080P needed.&lt;/P&gt;&lt;P&gt;when I set to splite mode,fb0 shows&lt;/P&gt;&lt;P&gt;&lt;IMG class="jiveImage" style="max-height: 900px; max-width: 1200px;" /&gt;cat mode:&lt;/P&gt;&lt;P&gt;U:1920*1080P-56&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but&amp;nbsp; I can't&amp;nbsp; measure the clk on the pin...so I can't understand it ,so strangely.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Apr 2014 06:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307284#M39669</guid>
      <dc:creator>leeo</dc:creator>
      <dc:date>2014-04-30T06:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: something  wrong with 1080P on IMX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307285#M39670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi liu,&lt;/P&gt;&lt;P&gt;i.MX53 supports (1866 x 1050 @60 frames per second) as&lt;/P&gt;&lt;P&gt;states sect.47.2.1 MX53 RM. "U:1920*1080P-56" is supported as well.&lt;/P&gt;&lt;P&gt;However for testing better to use OBDS, it is simpler and allows &lt;/P&gt;&lt;P&gt;easily to printf and modify regisers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMX53_QSB_OBDS "On-Board Diagnostic Suit for the i.MX53 Quick Start Board"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 May 2014 23:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307285#M39670</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-04T23:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Re: something  wrong with 1080P on IMX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307286#M39671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi chipexpert：&lt;/P&gt;&lt;P&gt;&amp;nbsp; we have requrement 1080P for&amp;nbsp; customer .&lt;/P&gt;&lt;P&gt;&amp;nbsp; I want to know why I can't measure the CLK of LVDS pin.&lt;/P&gt;&lt;P&gt; Please see attached file. Is there something wrong with sch? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2014 02:00:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/something-wrong-with-1080P-on-IMX535/m-p/307286#M39671</guid>
      <dc:creator>leeo</dc:creator>
      <dc:date>2014-05-05T02:00:59Z</dc:date>
    </item>
  </channel>
</rss>