<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 linux development</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306823#M39578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shahzad, we simply use mainline Linux kernel and buildroot to build a simple root file system to test out things on our sabre SD board.&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Apr 2014 17:06:26 GMT</pubDate>
    <dc:creator>sinanakman</dc:creator>
    <dc:date>2014-04-30T17:06:26Z</dc:date>
    <item>
      <title>iMX6 linux development</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306821#M39576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having some development system startup issues with ltib on the i.MX6.&amp;nbsp; I have seen that some people use yocto, which also is giving me headaches.&amp;nbsp; I would rather work at a low level, with the kernel source code and a functional file system, I am having problems getting a cross-compiled app to work with the existing linux SD cards that we have. What other paths are developers using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 19:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306821#M39576</guid>
      <dc:creator>Chicago1984</dc:creator>
      <dc:date>2014-04-29T19:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 linux development</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306822#M39577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Shahzad, your headaches are understandable :smileyhappy: Yocto is a completely different system but it is the way to go for integrating your packages/drivers. What are the specific problems you have? Are you using the cross-toolchain produced by bitbake?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 20:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306822#M39577</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2014-04-29T20:48:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 linux development</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306823#M39578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shahzad, we simply use mainline Linux kernel and buildroot to build a simple root file system to test out things on our sabre SD board.&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Apr 2014 17:06:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306823#M39578</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2014-04-30T17:06:26Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 linux development</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306824#M39579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following may be helpful for Linux applications development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"AN3870&amp;nbsp; Developing an Application for the i.MX Devices on Linux Platform"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf"&gt;http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The next app note may be useful in debugging :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 May 2014 05:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-linux-development/m-p/306824#M39579</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-05-06T05:13:00Z</dc:date>
    </item>
  </channel>
</rss>