<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The solution for the USB test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306576#M39500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Apr 2014 03:53:44 GMT</pubDate>
    <dc:creator>george</dc:creator>
    <dc:date>2014-04-01T03:53:44Z</dc:date>
    <item>
      <title>The solution for the USB test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306573#M39497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to verify USB-I/F for the i.MX6 original board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Isn't the utility for a USB compliance test in somewhere?&lt;/P&gt;&lt;P&gt;* I use USB as a host on linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there are some good ideas, please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 02:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306573#M39497</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2014-03-31T02:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: The solution for the USB test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306574#M39498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please note that there is no special software needed to generate the&lt;/P&gt;&lt;P&gt;test pattern. The USB controller is compliant with the EHCI specification.&lt;/P&gt;&lt;P&gt;The test modes are set by the PTC bits in the PORTSC register (bits 19-16).&lt;/P&gt;&lt;P&gt;PTC = 0x4 will force the controller to send the test packet.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Prior to setting the test mode, the controller must be initialized in the same&lt;/P&gt;&lt;P&gt;way as for normal operation. If the controller is running, the driver must first&lt;/P&gt;&lt;P&gt;stop the asynchronous and synchronous schedules and stop the controller&lt;/P&gt;&lt;P&gt;(USBCMS.RS = 0).&lt;/P&gt;&lt;P&gt;Then the PTC bits can be set for the desired test mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 03:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306574#M39498</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-03-31T03:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: The solution for the USB test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306575#M39499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are referring to the PC software tool for the USB hub/device framework testing, please refer to the page &lt;A href="http://www.usb.org/developers/tools/" title="http://www.usb.org/developers/tools/"&gt;USB.org - Tools&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 07:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306575#M39499</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2014-03-31T07:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: The solution for the USB test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306576#M39500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 03:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306576#M39500</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2014-04-01T03:53:44Z</dc:date>
    </item>
    <item>
      <title>Re: The solution for the USB test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306577#M39501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Peter,&lt;/P&gt;&lt;P&gt;Thank you for your infomation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 03:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-solution-for-the-USB-test/m-p/306577#M39501</guid>
      <dc:creator>george</dc:creator>
      <dc:date>2014-04-01T03:55:52Z</dc:date>
    </item>
  </channel>
</rss>