<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Selecting a suitable i.MX6 development board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Selecting-a-suitable-i-MX6-development-board/m-p/306563#M39496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Afzal I believe Sabre Automotive board will most&lt;/P&gt;&lt;P&gt;suit for these purposes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;SABRE for Automotive Infotainment Based on the i.MX 6 Series&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Apr 2014 06:51:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-04-30T06:51:37Z</dc:date>
    <item>
      <title>Selecting a suitable i.MX6 development board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Selecting-a-suitable-i-MX6-development-board/m-p/306562#M39495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a requirement - a new WiFi device that can be connected through full size MMC/SD connector, needs to work in Linux on an i.MX6 platform. WiFi device also has an alternate mode of communicating through UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware requirements on development board,&lt;/P&gt;&lt;P&gt;1. full size MMC/SD slot (for connecting WiFi device)&lt;/P&gt;&lt;P&gt;2. Another full size MMC/SD or microSD slot - for the card with images for booting&lt;/P&gt;&lt;P&gt;3. debug UART&lt;/P&gt;&lt;P&gt;4. UART with flow control capabilities (for WiFi device at higher speed)&lt;/P&gt;&lt;P&gt;5. at least one LED that can be controlled via GPIO&lt;/P&gt;&lt;P&gt;6. USB OTG&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In software side, it would need to run DHCP, http server etc. on Linux, so may be an Ubuntu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest an i.MX6 development board that suits above hardware requirements and on which software sources (&amp;amp; support) are available so that we can quickly start developing WiFi driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I am new to Freescale things&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Afzal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 12:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Selecting-a-suitable-i-MX6-development-board/m-p/306562#M39495</guid>
      <dc:creator>afzalmohammed</dc:creator>
      <dc:date>2014-04-29T12:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: Selecting a suitable i.MX6 development board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Selecting-a-suitable-i-MX6-development-board/m-p/306563#M39496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Afzal I believe Sabre Automotive board will most&lt;/P&gt;&lt;P&gt;suit for these purposes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREAUTO&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;SABRE for Automotive Infotainment Based on the i.MX 6 Series&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Apr 2014 06:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Selecting-a-suitable-i-MX6-development-board/m-p/306563#M39496</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-30T06:51:37Z</dc:date>
    </item>
  </channel>
</rss>