<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX537 issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306222#M39413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually we never met similar issues before.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only can suspect that there is something wrong with the power&lt;BR /&gt;scheme or with processor power-up seqence. So the processor&lt;BR /&gt;does not start when you turned the power on and when you touch&lt;BR /&gt;the processor this small electric discharge stars the system up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for sample bring-up checklist for the board please refer&lt;BR /&gt;chapter 7 of i.MX53 System Development User's Guide.&lt;BR /&gt;You can perform the tasks listed in the table 7-2 &lt;BR /&gt;with and without finger. If you see some difference you&lt;BR /&gt;get an idea what exactly is going wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Apr 2014 08:51:14 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2014-04-01T08:51:14Z</dc:date>
    <item>
      <title>iMX537 issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306221#M39412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using iMX537 in my target board and finding peculiar problem while programming. In my target board whenever i am trying to program, iMX537 doesnt responds to the JTAG connectivity. &lt;/P&gt;&lt;P&gt;On doubting the BGA soldering, i pressed the BGA it started responding. Then i tried to reduce my contact pressure on the chip still it works. Later i tried on other 2 target boards found the similar behavior. There after i concluded that its not soldering issues. Even a simple touch will make the iMX537 to respond. One observation that i did was when ever i turn on the power to the board initially target board consumes 250mA @ 8.4V. Later when i touch the iMX537 the current consumption changes to 300mA @ 8.4V , It starts responding to JTAG even though i am not touching. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me solutions if someone has faced similar sort of issue in there design or is it any peculiar behavior of some iMX537 batch. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;P&gt;Chiru&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Mar 2014 15:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306221#M39412</guid>
      <dc:creator>chiranjeevimata</dc:creator>
      <dc:date>2014-03-28T15:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX537 issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306222#M39413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually we never met similar issues before.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only can suspect that there is something wrong with the power&lt;BR /&gt;scheme or with processor power-up seqence. So the processor&lt;BR /&gt;does not start when you turned the power on and when you touch&lt;BR /&gt;the processor this small electric discharge stars the system up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for sample bring-up checklist for the board please refer&lt;BR /&gt;chapter 7 of i.MX53 System Development User's Guide.&lt;BR /&gt;You can perform the tasks listed in the table 7-2 &lt;BR /&gt;with and without finger. If you see some difference you&lt;BR /&gt;get an idea what exactly is going wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 08:51:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306222#M39413</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2014-04-01T08:51:14Z</dc:date>
    </item>
    <item>
      <title>Re: iMX537 issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306223#M39414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using DA9053-3N for power sequencing. I checked the power up sequencing its meeting as per the Pageno112 of iMX53UG.pdf.&lt;/P&gt;&lt;P&gt;Also as mentioned in the earlier post, the only change that i found is that the board power consumption changes from 240mA to 270mA after touching.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have one doubt, Initially the JTAG_MODE was pulled up to 3.3V, when it was not getting detected i changed the pull-up to pull-down then JTAG started detecting only when i touch the processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know will JTAG_MODE pin will cause any problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chiranjeevi M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 11:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX537-issues/m-p/306223#M39414</guid>
      <dc:creator>chiranjeevimata</dc:creator>
      <dc:date>2014-04-01T11:32:53Z</dc:date>
    </item>
  </channel>
</rss>