<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX53 - System reset when performing WiFi re-connect test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-System-reset-when-performing-WiFi-re-connect-test/m-p/306151#M39373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We bumped into a problem while doing WiFi re-connect test.&lt;/P&gt;&lt;P&gt;The test is simple, under Android, connect to an Access Point or Router, then disconnect it, then re-connect, then disconnect and keep looping this process.&lt;/P&gt;&lt;P&gt;Then after sometime, the system will suddenly reboot.&lt;/P&gt;&lt;P&gt;This problem doesn't occur very often, and not too easy to repeat.&lt;/P&gt;&lt;P&gt;But we would like to at least know the reason behind it and see if there is any fix.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Android 2.3.4,, which is based on BSP R10.3.2 on a iMX53 platform.&lt;/P&gt;&lt;P&gt;We are using a WiFi module that uses Marvell 88W8787 chipset, and the driver we uses is SD-UAPSTA-BT-FM-8787-LINUX2635-PXA920-14.66.9.p92-M2614322_AX-GPL.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is part of the log file when the reset problem occurs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.927 2014] The raw data count is 76 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.937 2014] The OS data count is 14 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.937 2014] PEN UP DECLARED &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.353 2014] Timeout cmd id (1400777140.720837) = 0xa9, act = 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.363 2014] a9 00 08 00 01 00 00 00 00 00 00 00 00 00 00 00 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] BSS type = 0 BSS role= 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] num_cmd_timeout = 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] last_cmd_index = 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] last_cmd_id = 0x0 0xa9 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_act = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_resp_index = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_resp_id = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] last_event_index = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] last_event = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] num_data_h2c_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_cmd_h2c_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_data_c2h_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_cmdevt_c2h_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_int_read_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] last_int_status = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_deauth = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_disassoc = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_link_lost = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_cmd_deauth = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_cmd_assoc_success = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] num_cmd_assoc_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] cmd_resp_received=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] event_received=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] max_tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] curr_tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] data_sent=1 cmd_sent=1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] ps_mode=1 ps_state=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] wakeup_dev_req=0 wakeup_tries=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] hs_configured=0 hs_activated=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] pps_uapsd_mode=0 sleep_pd=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] tx_lock_flag = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] scan_processing = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] mp_rd_bitmap=0x0 curr_rd_port=0x1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] mp_wr_bitmap=0x0 curr_wr_port=0x1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] Driver version = SD8787-0.0.0.p0-M2614322-GPL-(FP66) &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] main_state = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] ioctl_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] tx_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] rx_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] malloc_count = 34&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] lock_count = 53&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] mbufalloc_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] hs_skip_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] hs_force_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014]&amp;nbsp; clk_enable cannot be called in an interrupt context&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.483 2014] [&amp;lt;c00905cc&amp;gt;] (unwind_backtrace+0x0/0xf0) from [&amp;lt;c009d4e4&amp;gt;] (clk_enable+0x34/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.483 2014] [&amp;lt;c009d4e4&amp;gt;] (clk_enable+0x34/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.494 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.504 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.504 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.514 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.524 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.534 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.534 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.544 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.544 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.554 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.564 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.614 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.644 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] kernel BUG at arch/arm/plat-mxc/clock.c:178!&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] pgd = c0004000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [00000000] *pgd=00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] Internal error: Oops: 817 [#1] PREEMPT&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.664 2014] last sysfs file: /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.664 2014] Modules linked in: sd8xxx(-) mlan(P) [last unloaded: mlan]&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] CPU: 0&amp;nbsp;&amp;nbsp;&amp;nbsp; Tainted: P&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (2.6.35.3-gf221a2c #1)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] PC is at __bug+0x18/0x24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] LR is at __bug+0x14/0x24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.684 2014] pc : [&amp;lt;c008ee90&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;c008ee8c&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; psr: 60000193&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.684 2014] sp : c91fbce0&amp;nbsp; ip : d50f2000&amp;nbsp; fp : 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.694 2014] r10: 00000000&amp;nbsp; r9 : c91fa000&amp;nbsp; r8 : 00000001&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.694 2014] r7 : 00000001&amp;nbsp; r6 : 00000000&amp;nbsp; r5 : 00000000&amp;nbsp; r4 : c0636904&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.704 2014] r3 : 00000000&amp;nbsp; r2 : c91fbcd4&amp;nbsp; r1 : c058a9c7&amp;nbsp; r0 : 00000033&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.704 2014] Flags: nZCv&amp;nbsp; IRQs off&amp;nbsp; FIQs on&amp;nbsp; Mode SVC_32&amp;nbsp; ISA ARM&amp;nbsp; Segment kernel&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.714 2014] Control: 10c5387d&amp;nbsp; Table: 8191c019&amp;nbsp; DAC: 00000017&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.714 2014] Process MOAL_WORK_QUEUE (pid: 17191, stack limit = 0xc91fa2e8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.724 2014] Stack: (0xc91fbce0 to 0xc91fc000)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.724 2014] bce0: c0636904 c009d4f0 d345d600 00000000 00000000 c0369754 d345d400 00000100&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.734 2014] bd00: 00000000 c03694b0 00000002 d345d600 00010002 d344ab00 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.734 2014] bd20: 00000002 00000001 c91fa000 00000000 00000000 c00e9a3c c063d044 00000002&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.744 2014] bd40: d344ab00 00000002 00000001 c00ebc34 00000002 00000000 00000001 c008b06c&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.754 2014] bd60: ffffffff d5000000 00000001 c008bacc 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.754 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.764 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff d345d600 d345d400&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.774 2014] bdc0: c91fbdfc c0369894 c91fbdfc d345d400 c91fbde0 c03609bc d345d400 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.774 2014] bde0: c91fbde0 c91fbde0 c91fbe34 d345d400 c91fbdfc c0360a34 e1a01007 c91fbe34&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.784 2014] be00: 00000000 00000000 c91fbddc c0360ae8 e3a03001 d345d400 00000000 c91fbe97&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.794 2014] be20: 00000001 c0364bd0 c91fbec8 00000000 bf32103e 00000034 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.794 2014] be40: 00000000 00000000 00000000 00000195 00000000 00000000 00000000 c91fbdfc&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.804 2014] be60: 00000000 c91fbf4c c91fbeb8 00000000 00000009 00000000 00000000 c91fbece&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.814 2014] be80: c948c600 c0365b3c 00000000 c91fbe97 c91fbf4c d1f30de0 00000000 bf2fca24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.814 2014] bea0: 00000009 e59a3000 e3130080 0a000001 0000003c 00000028 4f494453 6e754620&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.834 2014] bec0: 28203063 2d307830 29397830 0000203a 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.834 2014] bee0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.844 2014] bf00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.844 2014] bf20: 00000000 00000000 00000000 00000000 00000000 00000000 00000028 00000030&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.854 2014] bf40: 00000034 00000038 0000003c 00000000 d1a76300 c948c600 c948c720 d1f30be8&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.864 2014] bf60: bf2fcb38 c91fbf94 c948c724 00000000 c948c720 bf2fcb78 c948c720 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.864 2014] bf80: d1f30be0 c91fa000 d1f30be0 c00c5624 00000000 00000000 d1a76300 c00c8fc4&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.874 2014] bfa0: c91fbfa0 c91fbfa0 00000000 d31b3da8 c91fbfd4 c00c54a8 d1f30be0 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.884 2014] bfc0: 00000000 00000000 00000000 c00c8c90 00000000 00000000 c91fbfd8 c91fbfd8&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.884 2014] bfe0: 00000000 d31b3da8 c00c8c18 c008ca20 00000013 c008ca20 e1a01006 e1a02007&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.894 2014] [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24) from [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.904 2014] [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.904 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.914 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.924 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.934 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.934 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.944 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.944 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.954 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.964 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.974 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.974 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.984 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.994 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.994 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.004 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.014 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.024 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.034 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.044 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.054 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.054 2014] Code: e92d4010 e59f000c eb10ad8a e3a03000 (e5833000) &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.064 2014] ---[ end trace c73d515ea4ed09b9 ]---&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.064 2014] Kernel panic - not syncing: Fatal exception in interrupt&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.074 2014] [&amp;lt;c00905cc&amp;gt;] (unwind_backtrace+0x0/0xf0) from [&amp;lt;c04ba444&amp;gt;] (panic+0x6c/0xe0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.074 2014] [&amp;lt;c04ba444&amp;gt;] (panic+0x6c/0xe0) from [&amp;lt;c008f460&amp;gt;] (die+0x2b4/0x304)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.084 2014] [&amp;lt;c008f460&amp;gt;] (die+0x2b4/0x304) from [&amp;lt;c00913cc&amp;gt;] (__do_kernel_fault+0x64/0x84)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.094 2014] [&amp;lt;c00913cc&amp;gt;] (__do_kernel_fault+0x64/0x84) from [&amp;lt;c00915ac&amp;gt;] (do_page_fault+0x1c0/0x1d4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.094 2014] [&amp;lt;c00915ac&amp;gt;] (do_page_fault+0x1c0/0x1d4) from [&amp;lt;c008b2c8&amp;gt;] (do_DataAbort+0x34/0x94)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.104 2014] [&amp;lt;c008b2c8&amp;gt;] (do_DataAbort+0x34/0x94) from [&amp;lt;c008ba6c&amp;gt;] (__dabt_svc+0x4c/0x60)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.114 2014] Exception stack(0xc91fbc98 to 0xc91fbce0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.114 2014] bc80:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000033 c058a9c7&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.124 2014] bca0: c91fbcd4 00000000 c0636904 00000000 00000000 00000001 00000001 c91fa000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.134 2014] bcc0: 00000000 00000000 d50f2000 c91fbce0 c008ee8c c008ee90 60000193 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.134 2014] [&amp;lt;c008ba6c&amp;gt;] (__dabt_svc+0x4c/0x60) from [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.144 2014] [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24) from [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.154 2014] [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.154 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.164 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.174 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.185 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.195 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.195 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.205 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.205 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.215 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.215 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.235 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.235 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.245 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.255 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.265 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.265 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.275 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.285 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.295 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.305 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] U-Boot 2009.08 ( 5月 21 2014 - 14:13:10)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX53 family 2.1V at 800 MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll1: 800MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll2: 394MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll3: 216MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll4: 455MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 65832000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ipg per clock : 32916000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 65832000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 54000000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 131664000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] axi_a clock&amp;nbsp;&amp;nbsp; : 394992000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] axi_b clock&amp;nbsp;&amp;nbsp; : 197496000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] emi_slow clock: 131664000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 394992000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc1 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc2 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc3 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc4 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 26332800Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Board: MX53-JJ08 Rev. A&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Boot Reason: [WDOG]&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Boot Device: MMC&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] DRAM:&amp;nbsp; 512 MB&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] MMC:&amp;nbsp;&amp;nbsp; FSL_ESDHC: 0, FSL_ESDHC: 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.210 2014] *** Warning - bad CRC or MMC, using default environment&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 May 2014 08:58:47 GMT</pubDate>
    <dc:creator>DonnyChiu</dc:creator>
    <dc:date>2014-05-27T08:58:47Z</dc:date>
    <item>
      <title>iMX53 - System reset when performing WiFi re-connect test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-System-reset-when-performing-WiFi-re-connect-test/m-p/306151#M39373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We bumped into a problem while doing WiFi re-connect test.&lt;/P&gt;&lt;P&gt;The test is simple, under Android, connect to an Access Point or Router, then disconnect it, then re-connect, then disconnect and keep looping this process.&lt;/P&gt;&lt;P&gt;Then after sometime, the system will suddenly reboot.&lt;/P&gt;&lt;P&gt;This problem doesn't occur very often, and not too easy to repeat.&lt;/P&gt;&lt;P&gt;But we would like to at least know the reason behind it and see if there is any fix.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using Android 2.3.4,, which is based on BSP R10.3.2 on a iMX53 platform.&lt;/P&gt;&lt;P&gt;We are using a WiFi module that uses Marvell 88W8787 chipset, and the driver we uses is SD-UAPSTA-BT-FM-8787-LINUX2635-PXA920-14.66.9.p92-M2614322_AX-GPL.zip&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is part of the log file when the reset problem occurs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.927 2014] The raw data count is 76 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.937 2014] The OS data count is 14 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:35.937 2014] PEN UP DECLARED &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.353 2014] Timeout cmd id (1400777140.720837) = 0xa9, act = 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.363 2014] a9 00 08 00 01 00 00 00 00 00 00 00 00 00 00 00 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] BSS type = 0 BSS role= 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] num_cmd_timeout = 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] last_cmd_index = 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.373 2014] last_cmd_id = 0x0 0xa9 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_act = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_resp_index = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.383 2014] last_cmd_resp_id = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] last_event_index = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] last_event = 0x0 0x0 0x0 0x0 0x0 &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.393 2014] num_data_h2c_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_cmd_h2c_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_data_c2h_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_cmdevt_c2h_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.403 2014] num_int_read_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] last_int_status = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_deauth = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_disassoc = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_event_link_lost = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_cmd_deauth = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.413 2014] num_cmd_assoc_success = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] num_cmd_assoc_failure = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] cmd_resp_received=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] event_received=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] max_tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.423 2014] tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] curr_tx_buf_size=2048&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] data_sent=1 cmd_sent=1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] ps_mode=1 ps_state=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] wakeup_dev_req=0 wakeup_tries=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.433 2014] hs_configured=0 hs_activated=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] pps_uapsd_mode=0 sleep_pd=0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] tx_lock_flag = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] scan_processing = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] mp_rd_bitmap=0x0 curr_rd_port=0x1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.443 2014] mp_wr_bitmap=0x0 curr_wr_port=0x1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] Driver version = SD8787-0.0.0.p0-M2614322-GPL-(FP66) &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] main_state = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.453 2014] ioctl_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] tx_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] rx_pending = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] malloc_count = 34&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.463 2014] lock_count = 53&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] mbufalloc_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] hs_skip_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014] hs_force_count = 0&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.473 2014]&amp;nbsp; clk_enable cannot be called in an interrupt context&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.483 2014] [&amp;lt;c00905cc&amp;gt;] (unwind_backtrace+0x0/0xf0) from [&amp;lt;c009d4e4&amp;gt;] (clk_enable+0x34/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.483 2014] [&amp;lt;c009d4e4&amp;gt;] (clk_enable+0x34/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.494 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.504 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.504 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.514 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.524 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.534 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.534 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.544 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.544 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.554 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.564 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.614 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.634 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.644 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] kernel BUG at arch/arm/plat-mxc/clock.c:178!&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] pgd = c0004000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] [00000000] *pgd=00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.654 2014] Internal error: Oops: 817 [#1] PREEMPT&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.664 2014] last sysfs file: /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.664 2014] Modules linked in: sd8xxx(-) mlan(P) [last unloaded: mlan]&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] CPU: 0&amp;nbsp;&amp;nbsp;&amp;nbsp; Tainted: P&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (2.6.35.3-gf221a2c #1)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] PC is at __bug+0x18/0x24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.674 2014] LR is at __bug+0x14/0x24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.684 2014] pc : [&amp;lt;c008ee90&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; lr : [&amp;lt;c008ee8c&amp;gt;]&amp;nbsp;&amp;nbsp;&amp;nbsp; psr: 60000193&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.684 2014] sp : c91fbce0&amp;nbsp; ip : d50f2000&amp;nbsp; fp : 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.694 2014] r10: 00000000&amp;nbsp; r9 : c91fa000&amp;nbsp; r8 : 00000001&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.694 2014] r7 : 00000001&amp;nbsp; r6 : 00000000&amp;nbsp; r5 : 00000000&amp;nbsp; r4 : c0636904&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.704 2014] r3 : 00000000&amp;nbsp; r2 : c91fbcd4&amp;nbsp; r1 : c058a9c7&amp;nbsp; r0 : 00000033&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.704 2014] Flags: nZCv&amp;nbsp; IRQs off&amp;nbsp; FIQs on&amp;nbsp; Mode SVC_32&amp;nbsp; ISA ARM&amp;nbsp; Segment kernel&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.714 2014] Control: 10c5387d&amp;nbsp; Table: 8191c019&amp;nbsp; DAC: 00000017&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.714 2014] Process MOAL_WORK_QUEUE (pid: 17191, stack limit = 0xc91fa2e8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.724 2014] Stack: (0xc91fbce0 to 0xc91fc000)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.724 2014] bce0: c0636904 c009d4f0 d345d600 00000000 00000000 c0369754 d345d400 00000100&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.734 2014] bd00: 00000000 c03694b0 00000002 d345d600 00010002 d344ab00 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.734 2014] bd20: 00000002 00000001 c91fa000 00000000 00000000 c00e9a3c c063d044 00000002&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.744 2014] bd40: d344ab00 00000002 00000001 c00ebc34 00000002 00000000 00000001 c008b06c&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.754 2014] bd60: ffffffff d5000000 00000001 c008bacc 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.754 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.764 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff d345d600 d345d400&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.774 2014] bdc0: c91fbdfc c0369894 c91fbdfc d345d400 c91fbde0 c03609bc d345d400 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.774 2014] bde0: c91fbde0 c91fbde0 c91fbe34 d345d400 c91fbdfc c0360a34 e1a01007 c91fbe34&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.784 2014] be00: 00000000 00000000 c91fbddc c0360ae8 e3a03001 d345d400 00000000 c91fbe97&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.794 2014] be20: 00000001 c0364bd0 c91fbec8 00000000 bf32103e 00000034 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.794 2014] be40: 00000000 00000000 00000000 00000195 00000000 00000000 00000000 c91fbdfc&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.804 2014] be60: 00000000 c91fbf4c c91fbeb8 00000000 00000009 00000000 00000000 c91fbece&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.814 2014] be80: c948c600 c0365b3c 00000000 c91fbe97 c91fbf4c d1f30de0 00000000 bf2fca24&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.814 2014] bea0: 00000009 e59a3000 e3130080 0a000001 0000003c 00000028 4f494453 6e754620&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.834 2014] bec0: 28203063 2d307830 29397830 0000203a 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.834 2014] bee0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.844 2014] bf00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.844 2014] bf20: 00000000 00000000 00000000 00000000 00000000 00000000 00000028 00000030&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.854 2014] bf40: 00000034 00000038 0000003c 00000000 d1a76300 c948c600 c948c720 d1f30be8&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.864 2014] bf60: bf2fcb38 c91fbf94 c948c724 00000000 c948c720 bf2fcb78 c948c720 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.864 2014] bf80: d1f30be0 c91fa000 d1f30be0 c00c5624 00000000 00000000 d1a76300 c00c8fc4&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.874 2014] bfa0: c91fbfa0 c91fbfa0 00000000 d31b3da8 c91fbfd4 c00c54a8 d1f30be0 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.884 2014] bfc0: 00000000 00000000 00000000 c00c8c90 00000000 00000000 c91fbfd8 c91fbfd8&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.884 2014] bfe0: 00000000 d31b3da8 c00c8c18 c008ca20 00000013 c008ca20 e1a01006 e1a02007&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.894 2014] [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24) from [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.904 2014] [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.904 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.914 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.924 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.934 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.934 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.944 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.944 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.954 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.964 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.974 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.974 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.984 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.994 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:40.994 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.004 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.014 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.024 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.034 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.044 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.054 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.054 2014] Code: e92d4010 e59f000c eb10ad8a e3a03000 (e5833000) &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.064 2014] ---[ end trace c73d515ea4ed09b9 ]---&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.064 2014] Kernel panic - not syncing: Fatal exception in interrupt&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.074 2014] [&amp;lt;c00905cc&amp;gt;] (unwind_backtrace+0x0/0xf0) from [&amp;lt;c04ba444&amp;gt;] (panic+0x6c/0xe0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.074 2014] [&amp;lt;c04ba444&amp;gt;] (panic+0x6c/0xe0) from [&amp;lt;c008f460&amp;gt;] (die+0x2b4/0x304)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.084 2014] [&amp;lt;c008f460&amp;gt;] (die+0x2b4/0x304) from [&amp;lt;c00913cc&amp;gt;] (__do_kernel_fault+0x64/0x84)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.094 2014] [&amp;lt;c00913cc&amp;gt;] (__do_kernel_fault+0x64/0x84) from [&amp;lt;c00915ac&amp;gt;] (do_page_fault+0x1c0/0x1d4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.094 2014] [&amp;lt;c00915ac&amp;gt;] (do_page_fault+0x1c0/0x1d4) from [&amp;lt;c008b2c8&amp;gt;] (do_DataAbort+0x34/0x94)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.104 2014] [&amp;lt;c008b2c8&amp;gt;] (do_DataAbort+0x34/0x94) from [&amp;lt;c008ba6c&amp;gt;] (__dabt_svc+0x4c/0x60)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.114 2014] Exception stack(0xc91fbc98 to 0xc91fbce0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.114 2014] bc80:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000033 c058a9c7&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.124 2014] bca0: c91fbcd4 00000000 c0636904 00000000 00000000 00000001 00000001 c91fa000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.134 2014] bcc0: 00000000 00000000 d50f2000 c91fbce0 c008ee8c c008ee90 60000193 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.134 2014] [&amp;lt;c008ba6c&amp;gt;] (__dabt_svc+0x4c/0x60) from [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.144 2014] [&amp;lt;c008ee90&amp;gt;] (__bug+0x18/0x24) from [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.154 2014] [&amp;lt;c009d4f0&amp;gt;] (clk_enable+0x40/0x158) from [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.154 2014] [&amp;lt;c0369754&amp;gt;] (sdhci_enable_sdio_irq+0x24/0x140) from [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.164 2014] [&amp;lt;c03694b0&amp;gt;] (sdhci_irq+0x778/0x7b0) from [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.174 2014] [&amp;lt;c00e9a3c&amp;gt;] (handle_IRQ_event+0x24/0xe4) from [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.185 2014] [&amp;lt;c00ebc34&amp;gt;] (handle_level_irq+0xdc/0x188) from [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.195 2014] [&amp;lt;c008b06c&amp;gt;] (asm_do_IRQ+0x6c/0x8c) from [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.195 2014] Exception stack(0xc91fbd70 to 0xc91fbdb8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.205 2014] bd60:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 00000000 00f0003f c91fbdb8 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.205 2014] bd80: 00000000 40000013 c91fbdfc 00000000 00000000 c91fbe34 00000000 00000000&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.215 2014] bda0: 00000003 c91fbdb8 c009d304 c009d5c0 60000013 ffffffff&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.215 2014] [&amp;lt;c008bacc&amp;gt;] (__irq_svc+0x4c/0xcc) from [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.235 2014] [&amp;lt;c009d5c0&amp;gt;] (clk_enable+0x110/0x158) from [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.235 2014] [&amp;lt;c0369894&amp;gt;] (sdhci_request+0x24/0x154) from [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.245 2014] [&amp;lt;c03609bc&amp;gt;] (mmc_wait_for_req+0x118/0x12c) from [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.255 2014] [&amp;lt;c0360a34&amp;gt;] (mmc_wait_for_cmd+0x64/0x74) from [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.265 2014] [&amp;lt;c0364bd0&amp;gt;] (mmc_io_rw_direct_host+0xc0/0x124) from [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.265 2014] [&amp;lt;c0365b3c&amp;gt;] (sdio_f0_readb+0x4c/0x74) from [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.275 2014] [&amp;lt;bf2fca24&amp;gt;] (woal_sdio_reg_dbg+0x104/0x218 [sd8xxx]) from [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx])&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.285 2014] [&amp;lt;bf2fcb78&amp;gt;] (woal_main_work_queue+0x40/0xf8 [sd8xxx]) from [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.295 2014] [&amp;lt;c00c5624&amp;gt;] (worker_thread+0x17c/0x228) from [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:41.305 2014] [&amp;lt;c00c8c90&amp;gt;] (kthread+0x78/0x80) from [&amp;lt;c008ca20&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:44.830 2014] U-Boot 2009.08 ( 5月 21 2014 - 14:13:10)&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] &lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX53 family 2.1V at 800 MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll1: 800MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll2: 394MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll3: 216MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] mx53 pll4: 455MHz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 65832000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ipg per clock : 32916000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 65832000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 54000000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 131664000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] axi_a clock&amp;nbsp;&amp;nbsp; : 394992000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] axi_b clock&amp;nbsp;&amp;nbsp; : 197496000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] emi_slow clock: 131664000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 394992000Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc1 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc2 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc3 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] esdhc4 clock&amp;nbsp; : 78998400Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 26332800Hz&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Board: MX53-JJ08 Rev. A&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Boot Reason: [WDOG]&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] Boot Device: MMC&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] DRAM:&amp;nbsp; 512 MB&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.030 2014] MMC:&amp;nbsp;&amp;nbsp; FSL_ESDHC: 0, FSL_ESDHC: 1&lt;/P&gt;&lt;P&gt;[Thu May 22 16:49:45.210 2014] *** Warning - bad CRC or MMC, using default environment&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 08:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-System-reset-when-performing-WiFi-re-connect-test/m-p/306151#M39373</guid>
      <dc:creator>DonnyChiu</dc:creator>
      <dc:date>2014-05-27T08:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 - System reset when performing WiFi re-connect test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-System-reset-when-performing-WiFi-re-connect-test/m-p/306152#M39374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;from the log, the reboot reason is a WDOG reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;firstly please check the software why the system send out a WDOG reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also please check the 32.768k crystal to see if it's stable when rebooting.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 09:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-System-reset-when-performing-WiFi-re-connect-test/m-p/306152#M39374</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-05-27T09:25:10Z</dc:date>
    </item>
  </channel>
</rss>