<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCPU load is getting upto 50% when USB Camera is used</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306141#M39369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When external USB camera is used for preview or recording (VGA resolution) CPU load is shooting up to 50% where as with internal camera it is only using 5%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to reduce CPU load for USB camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our use case, CPU load is going up to 97% when we use USB camera during VOIP video call, which involves&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Displaying own preview from USB camera&lt;/LI&gt;&lt;LI&gt;Displaying remote party video&lt;/LI&gt;&lt;LI&gt;VPU H264 encoding (from USB camera)&lt;/LI&gt;&lt;LI&gt;VPU H264 Decoding (remote party video). &lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where as for internal camera cpu usage is up to 75%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In practical, USB camera is not usable along with above operations for long duration calls due to high CPU usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know if there is any optimization possible to reduce CPU load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board: IMX6 SabreSD quad core&lt;/P&gt;&lt;P&gt;Android: 4.2.2.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 May 2014 09:33:37 GMT</pubDate>
    <dc:creator>mghasan</dc:creator>
    <dc:date>2014-05-27T09:33:37Z</dc:date>
    <item>
      <title>CPU load is getting upto 50% when USB Camera is used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306141#M39369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When external USB camera is used for preview or recording (VGA resolution) CPU load is shooting up to 50% where as with internal camera it is only using 5%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to reduce CPU load for USB camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our use case, CPU load is going up to 97% when we use USB camera during VOIP video call, which involves&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Displaying own preview from USB camera&lt;/LI&gt;&lt;LI&gt;Displaying remote party video&lt;/LI&gt;&lt;LI&gt;VPU H264 encoding (from USB camera)&lt;/LI&gt;&lt;LI&gt;VPU H264 Decoding (remote party video). &lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where as for internal camera cpu usage is up to 75%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In practical, USB camera is not usable along with above operations for long duration calls due to high CPU usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know if there is any optimization possible to reduce CPU load.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board: IMX6 SabreSD quad core&lt;/P&gt;&lt;P&gt;Android: 4.2.2.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 09:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306141#M39369</guid>
      <dc:creator>mghasan</dc:creator>
      <dc:date>2014-05-27T09:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: CPU load is getting upto 50% when USB Camera is used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306142#M39370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USB camera interface is not optimized , it is doing software color conversion for preview frame and frames to be encoded. Because of these two CSC load on CPU is too high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 09:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306142#M39370</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-05-27T09:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: CPU load is getting upto 50% when USB Camera is used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306143#M39371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Saurabh.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please suggest on how to use HW CSC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 May 2014 10:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306143#M39371</guid>
      <dc:creator>mghasan</dc:creator>
      <dc:date>2014-05-27T10:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: CPU load is getting upto 50% when USB Camera is used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306144#M39372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Hasan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to use IPU task to do the HW CSC.&lt;/P&gt;&lt;P&gt;Please check IPU example which will help you to implement it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 May 2014 03:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CPU-load-is-getting-upto-50-when-USB-Camera-is-used/m-p/306144#M39372</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-05-30T03:42:12Z</dc:date>
    </item>
  </channel>
</rss>