<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX28 with 2 Codecs in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305611#M39250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the iMX28 evalboard there is one codec connected to both iMX28 SAIF interfaces (SAIF0 for clk and transmit data, SAIF1 for receiving data). As we need to individual audio players we have two codecs, one connected to SAIF0 and one to SAIF1. Unfortunately Freescale's BSP does not support two codecs. Has anyone a solution for this or can support us?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Apr 2014 16:20:27 GMT</pubDate>
    <dc:creator>michaelkoelbl</dc:creator>
    <dc:date>2014-04-28T16:20:27Z</dc:date>
    <item>
      <title>iMX28 with 2 Codecs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305611#M39250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the iMX28 evalboard there is one codec connected to both iMX28 SAIF interfaces (SAIF0 for clk and transmit data, SAIF1 for receiving data). As we need to individual audio players we have two codecs, one connected to SAIF0 and one to SAIF1. Unfortunately Freescale's BSP does not support two codecs. Has anyone a solution for this or can support us?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 16:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305611#M39250</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2014-04-28T16:20:27Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 with 2 Codecs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305612#M39251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We can help you. We can customize the BSP for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please get in touch if you have interest.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 19:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305612#M39251</guid>
      <dc:creator>OtavioSalvador</dc:creator>
      <dc:date>2014-04-28T19:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX28 with 2 Codecs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305613#M39252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to use SAIF0 and SAIF1 interfaces independently in Linux 3.x or 4.x? As written above we want to connect two codecs both in playback mode. We made some attempts modifying the device tree of Mainline kernel 3.x but had no success. When checking the iMX28 registers we saw that we were able to initialize the pins as required but neither SAIF1-clock was initialized in the iMX28 clock distribution nor the SAIF1 control register was initialized. :-(&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2015 16:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX28-with-2-Codecs/m-p/305613#M39252</guid>
      <dc:creator>michaelkoelbl</dc:creator>
      <dc:date>2015-07-20T16:01:59Z</dc:date>
    </item>
  </channel>
</rss>