<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PF0100 question in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/305602#M39245</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John&lt;/P&gt;&lt;P&gt;yes, startup sequence is not determined by power good status of individual regulators.&lt;/P&gt;&lt;P&gt;However there is fault mode (described on p.17 MMPF0100 Datasheet).&lt;/P&gt;&lt;P&gt;If fault occurs and persists for 1.8 ms typically, RESETBMCU is asserted, LOW.&lt;/P&gt;&lt;P&gt;After 100 ms typically part will power off. To enter the fault mode, set bit &lt;/P&gt;&lt;P&gt;OTP_PG_EN of register OTP PWRGD EN to 1.&lt;/P&gt;&lt;P&gt;Also p.35 tells that each buck regulator has a programmable current limit. &lt;/P&gt;&lt;P&gt;In an overcurrent condition, if the current limit condition persists for more than &lt;/P&gt;&lt;P&gt;8.0 ms, a fault condition is generated.&lt;/P&gt;&lt;P&gt;LDOs have REGSCPEN bit, if REGSCPEN=1 LDO will be disabled.&lt;/P&gt;&lt;P&gt;Default REGSCPEN=0 (current limit), check p.84&lt;/P&gt;&lt;P&gt;MMPF0100 Datasheet (rev.6, 8/2013)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Mar 2014 10:04:57 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-03-31T10:04:57Z</dc:date>
    <item>
      <title>PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/305601#M39244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: black; font-family: 'Times New Roman','serif'; font-size: 10pt; mso-fareast-font-family: 'Times New Roman'; mso-ansi-language: EN-US; mso-fareast-language: ZH-CN; mso-bidi-language: AR-SA;"&gt;In section 6.1.2.1 of the datasheet, it seems that the startup sequence is determined by timeslot only, not the power good status of individual regulators.&amp;nbsp; If I wanted a sequence such as SW1 - SW3 - SW4 - SW2, a register must exist to specify that SW3's&lt;BR /&gt;turn-on event is the power-good status of SW1, but this register does not seem to exist.&lt;BR /&gt;&lt;BR /&gt;Can you confirm that this is the case?&amp;nbsp; If it is, the startup sequence will continue regardless of whether each individual regulator has reached its power good status or not.&amp;nbsp; In the above example, if SW3*IN is still at 0V when SW4 has already started, the power-on sequence will not work.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Mar 2014 01:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/305601#M39244</guid>
      <dc:creator>jwu</dc:creator>
      <dc:date>2014-03-28T01:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/305602#M39245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, John&lt;/P&gt;&lt;P&gt;yes, startup sequence is not determined by power good status of individual regulators.&lt;/P&gt;&lt;P&gt;However there is fault mode (described on p.17 MMPF0100 Datasheet).&lt;/P&gt;&lt;P&gt;If fault occurs and persists for 1.8 ms typically, RESETBMCU is asserted, LOW.&lt;/P&gt;&lt;P&gt;After 100 ms typically part will power off. To enter the fault mode, set bit &lt;/P&gt;&lt;P&gt;OTP_PG_EN of register OTP PWRGD EN to 1.&lt;/P&gt;&lt;P&gt;Also p.35 tells that each buck regulator has a programmable current limit. &lt;/P&gt;&lt;P&gt;In an overcurrent condition, if the current limit condition persists for more than &lt;/P&gt;&lt;P&gt;8.0 ms, a fault condition is generated.&lt;/P&gt;&lt;P&gt;LDOs have REGSCPEN bit, if REGSCPEN=1 LDO will be disabled.&lt;/P&gt;&lt;P&gt;Default REGSCPEN=0 (current limit), check p.84&lt;/P&gt;&lt;P&gt;MMPF0100 Datasheet (rev.6, 8/2013)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 10:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-question/m-p/305602#M39245</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-03-31T10:04:57Z</dc:date>
    </item>
  </channel>
</rss>