<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304962#M39038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dipen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this is possible, however it may depend on desired fps (framerate).&lt;/P&gt;&lt;P&gt;CSI performance is given in sect.37.1.2.1.1 "Camera Ports"&lt;/P&gt;&lt;P&gt;i.MX6DQ Reference Manual (rev.1&amp;nbsp; 4/2013)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"For parallel interface, the maximum speed of the interface is 240Mhz. The required&lt;/P&gt;&lt;P&gt;operating frequency of the interface is calculated in the following way:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF&lt;/P&gt;&lt;P&gt;Where&lt;/P&gt;&lt;P&gt;• FH = frame height (in pixels)&lt;/P&gt;&lt;P&gt;• FW = Frame width (in pixels)&lt;/P&gt;&lt;P&gt;• fps = frame rate (frames per second)&lt;/P&gt;&lt;P&gt;• BI = typically 35% overhead, should be assumed as 1.35. The actual blanking&lt;/P&gt;&lt;P&gt;intervals are a parameter of the attached device.&lt;/P&gt;&lt;P&gt;• DF = data format, defines the number of cycles needed to send a single pixel."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For two two camera at 1280x720p@30fps it would require about 60MHz (assume 1 cycle/pixel).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;H264 encode 720p@30fps two instances are possible with i.MX6DQ, please check p.31&lt;/P&gt;&lt;P&gt;presentation below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf" title="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf"&gt;http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Apr 2014 10:07:59 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-04-28T10:07:59Z</dc:date>
    <item>
      <title>Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304961#M39037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-size: 14px; margin-bottom: 10px; color: #555555; font-family: Georgia, 'Times New Roman', Times, serif; background-position: initial;"&gt;Is it possible to capture 2 simultaneous 1280x720p stream from two cameras on i.MX6 Dual/Quad?&lt;/P&gt;&lt;P style="font-size: 14px; margin-bottom: 10px; color: #555555; font-family: Georgia, 'Times New Roman', Times, serif; background-position: initial;"&gt;My goal is simultaneous capture from two camera at 1280x720p resolution and perform H.264 encoding and stream or store.&lt;/P&gt;&lt;P style="font-size: 14px; margin-bottom: 10px; color: #555555; font-family: Georgia, 'Times New Roman', Times, serif; background-position: initial;"&gt;Appreciate your earliest response.&lt;/P&gt;&lt;P style="font-size: 14px; margin-bottom: 10px; color: #555555; font-family: Georgia, 'Times New Roman', Times, serif; background-position: initial;"&gt;Regards,&lt;/P&gt;&lt;P style="font-size: 14px; margin-bottom: 10px; color: #555555; font-family: Georgia, 'Times New Roman', Times, serif; background-position: initial;"&gt;Dipen Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 06:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304961#M39037</guid>
      <dc:creator>DipenPatel1z</dc:creator>
      <dc:date>2014-04-28T06:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304962#M39038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dipen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, this is possible, however it may depend on desired fps (framerate).&lt;/P&gt;&lt;P&gt;CSI performance is given in sect.37.1.2.1.1 "Camera Ports"&lt;/P&gt;&lt;P&gt;i.MX6DQ Reference Manual (rev.1&amp;nbsp; 4/2013)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"For parallel interface, the maximum speed of the interface is 240Mhz. The required&lt;/P&gt;&lt;P&gt;operating frequency of the interface is calculated in the following way:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF&lt;/P&gt;&lt;P&gt;Where&lt;/P&gt;&lt;P&gt;• FH = frame height (in pixels)&lt;/P&gt;&lt;P&gt;• FW = Frame width (in pixels)&lt;/P&gt;&lt;P&gt;• fps = frame rate (frames per second)&lt;/P&gt;&lt;P&gt;• BI = typically 35% overhead, should be assumed as 1.35. The actual blanking&lt;/P&gt;&lt;P&gt;intervals are a parameter of the attached device.&lt;/P&gt;&lt;P&gt;• DF = data format, defines the number of cycles needed to send a single pixel."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For two two camera at 1280x720p@30fps it would require about 60MHz (assume 1 cycle/pixel).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;H264 encode 720p@30fps two instances are possible with i.MX6DQ, please check p.31&lt;/P&gt;&lt;P&gt;presentation below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf" title="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf"&gt;http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0223.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 10:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304962#M39038</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-28T10:07:59Z</dc:date>
    </item>
    <item>
      <title>Re: Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304963#M39039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chipexpert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for quick response and precise information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I can capture two camera streams of 720P@&lt;STRONG&gt;60fps&lt;/STRONG&gt; (~166MHz).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But encode will be &lt;STRONG&gt;limited to 720P@30fps for two instances. &lt;/STRONG&gt;Please confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dipen Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 11:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304963#M39039</guid>
      <dc:creator>DipenPatel1z</dc:creator>
      <dc:date>2014-04-29T11:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304964#M39040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you solve it? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 03:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304964#M39040</guid>
      <dc:creator>yangthomas</dc:creator>
      <dc:date>2014-07-10T03:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: Two simultaneous camera capture at 720p resolution, encode and stream with i.MX6 Dual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304965#M39041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dipen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 04:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Two-simultaneous-camera-capture-at-720p-resolution-encode-and/m-p/304965#M39041</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-07-10T04:27:14Z</dc:date>
    </item>
  </channel>
</rss>