<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mini-pcie clock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304928#M39021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Xiaoqiang &lt;/P&gt;&lt;P&gt;clock signal(100MHz) on pins (REFCLK- and REFCLK+)&amp;nbsp; is optional&lt;/P&gt;&lt;P&gt;signal, not all PCIe cards are using it. Freescale i.MX6 BSPs use &lt;/P&gt;&lt;P&gt;125MHz as this signal. You can add external 100MHz clock or try to find &lt;/P&gt;&lt;P&gt;card which does not require this signal. Some cards are mentioned&lt;/P&gt;&lt;P&gt;in Release Notes in Doc bundle, link below. Also please check &lt;/P&gt;&lt;P&gt;i.MX_6Dual6Quad_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;document sect.35.2.2 "Kernel configurations".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"L3.0.35_4.1.0_LINUX_DOCS "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Mar 2014 08:15:51 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2014-03-31T08:15:51Z</dc:date>
    <item>
      <title>mini-pcie clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304927#M39020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My platform is IMX6Q-SDP and linux BSP version is  L3.0.35_4.1.0_130816. Now I am testing Mini-PCIe wifi module(iwl4965) founction.&lt;/P&gt;&lt;P&gt;Support for iwl4965 is added in kernel driver.&lt;/P&gt;&lt;P&gt;A problem is that if I configure kernel like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale MXC Implementations  ---&amp;gt;&lt;/P&gt;&lt;P&gt;  PCI Express support&lt;/P&gt;&lt;P&gt;       PCI Express EP mode in the IMX6 RC/EP interconnection system   &lt;/P&gt;&lt;P&gt;       PCI Express RC mode in the IMX6 RC/EP interconnection system&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can detect clock signal(100MHz) on pin11 and 13(REFCLK- and REFCLK+) during boot up. But they only lasts for about one secend&lt;/P&gt;&lt;P&gt;and then disappear.And PCIe link up failed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I configure like this:&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Freescale MXC Implementations  ---&amp;gt;&lt;/P&gt;&lt;P&gt;  PCI Express support&lt;/P&gt;&lt;P&gt;       PCI Express EP mode in the IMX6 RC/EP interconnection system   &lt;/P&gt;&lt;P&gt;       PCI Express RC mode in the IMX6 RC/EP interconnection system&lt;/P&gt;&lt;P&gt;I can't get anly  clock signal on those pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the above can't make my pcie work and give the same error:&lt;/P&gt;&lt;P&gt;iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.&lt;/P&gt;&lt;P&gt;PCIE: imx_pcie_pltfm_probe start link up.&lt;/P&gt;&lt;P&gt;link up failed, DB_R0:0x00571600, DB_R1:0x08200000!&lt;/P&gt;&lt;P&gt;IMX PCIe port: link down!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Who can help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 03:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304927#M39020</guid>
      <dc:creator>xiaoqiangyang</dc:creator>
      <dc:date>2014-03-27T03:02:24Z</dc:date>
    </item>
    <item>
      <title>Re: mini-pcie clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304928#M39021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Xiaoqiang &lt;/P&gt;&lt;P&gt;clock signal(100MHz) on pins (REFCLK- and REFCLK+)&amp;nbsp; is optional&lt;/P&gt;&lt;P&gt;signal, not all PCIe cards are using it. Freescale i.MX6 BSPs use &lt;/P&gt;&lt;P&gt;125MHz as this signal. You can add external 100MHz clock or try to find &lt;/P&gt;&lt;P&gt;card which does not require this signal. Some cards are mentioned&lt;/P&gt;&lt;P&gt;in Release Notes in Doc bundle, link below. Also please check &lt;/P&gt;&lt;P&gt;i.MX_6Dual6Quad_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;document sect.35.2.2 "Kernel configurations".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"L3.0.35_4.1.0_LINUX_DOCS "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 08:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304928#M39021</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-03-31T08:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: mini-pcie clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304929#M39022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi chipexpert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My kernel is built acording to the manual, but it is of no help.Now I think something is wrong with the hardware.Because the pcie have been ok before and suddenly&lt;/P&gt;&lt;P&gt;broken down.So I will check my hardware. Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2014 01:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304929#M39022</guid>
      <dc:creator>xiaoqiangyang</dc:creator>
      <dc:date>2014-04-04T01:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: mini-pcie clock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304930#M39023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;have some one drive 4965 wifi card successfully?&lt;/P&gt;&lt;P&gt;i configed the kernel as others do ,but has no effect.&lt;/P&gt;&lt;P&gt;does it need clk ?&lt;/P&gt;&lt;P&gt;is the power votage 3.3V? &amp;nbsp;i use asm1117-3.3V to supply it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Nov 2017 00:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mini-pcie-clock/m-p/304930#M39023</guid>
      <dc:creator>jianminli</dc:creator>
      <dc:date>2017-11-29T00:15:25Z</dc:date>
    </item>
  </channel>
</rss>