<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304832#M38979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The u-boot has a board configuration file which has DCD data in the following format. &lt;/P&gt;&lt;P&gt;ADDRESS-TYPE&amp;nbsp; ADDRESS&amp;nbsp; VALUE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the IOMux Tool to configure the IOMUX.&lt;/P&gt;&lt;P&gt;Is there a easy way to generate the DCD data from the IOMux Tool? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Siva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 24 May 2014 01:45:16 GMT</pubDate>
    <dc:creator>sivaalagarsamy</dc:creator>
    <dc:date>2014-05-24T01:45:16Z</dc:date>
    <item>
      <title>Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304832#M38979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The u-boot has a board configuration file which has DCD data in the following format. &lt;/P&gt;&lt;P&gt;ADDRESS-TYPE&amp;nbsp; ADDRESS&amp;nbsp; VALUE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the IOMux Tool to configure the IOMUX.&lt;/P&gt;&lt;P&gt;Is there a easy way to generate the DCD data from the IOMux Tool? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Siva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 May 2014 01:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304832#M38979</guid>
      <dc:creator>sivaalagarsamy</dc:creator>
      <dc:date>2014-05-24T01:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304833#M38980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siva&lt;/P&gt;&lt;P&gt;there is no way for automatic DCD generation from&lt;/P&gt;&lt;P&gt;IOMUX tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 03:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304833#M38980</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-26T03:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304834#M38981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there another way to generate DCD data ?&lt;/P&gt;&lt;P&gt;Do you have examples DCD for various DDR hardware configurations or an application note dealing with ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mine is single chip MT41K128M16 (16M*16*8banks = 256MB) and I try to load correct configuration without success for the moment ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 16:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304834#M38981</guid>
      <dc:creator>mchaplet</dc:creator>
      <dc:date>2014-08-05T16:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304835#M38982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;probably links below may help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="331721" data-objecttype="2" href="https://community.freescale.com/message/331721#331721"&gt;https://community.freescale.com/message/331721#331721&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="32294" data-containertype="2020" data-objectid="96412" data-objecttype="102" href="https://community.freescale.com/docs/DOC-96412"&gt;https://community.freescale.com/docs/DOC-96412&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 23:59:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304835#M38982</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-08-05T23:59:29Z</dc:date>
    </item>
    <item>
      <title>Re: Generating the DCD (Device Configuration Data) for u-boot in IOMux Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304836#M38983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, It helps a lot !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a note, for other new designs : Don't forget to use MX6_MMDC_P0_MPODTCTRL = 0x00011117&amp;nbsp; instead default 22227 generated by script aid XLS.&lt;/P&gt;&lt;P&gt;I've found it "recommanded for new designs" in MX6DL_SabreSD_DDR3_register_programming_aid_v1.5.inc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 10:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Generating-the-DCD-Device-Configuration-Data-for-u-boot-in-IOMux/m-p/304836#M38983</guid>
      <dc:creator>mchaplet</dc:creator>
      <dc:date>2014-08-26T10:10:21Z</dc:date>
    </item>
  </channel>
</rss>