<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: using android w/o HW sound</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/using-android-w-o-HW-sound/m-p/304529#M38886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you need to modified hardware/imx to remove sound card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Mar 2014 13:43:36 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2014-03-26T13:43:36Z</dc:date>
    <item>
      <title>using android w/o HW sound</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-android-w-o-HW-sound/m-p/304528#M38885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We made a spinoff of a Boundary Nitrogen6q board, we removed the SGTL5000 audio codec chip, we also set BOARD_HAS_SGTL5000 := false in the BoardConfig.mk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However in Android logcat we see a lot of :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2372): card -1, port 0 device 0x2&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2372): rate 44100, channel 2 period_size 0xc0&lt;/P&gt;&lt;P&gt;E/audio_hw_primary( 2372): cannot open pcm_out driver 0: cannot open device '/dev/snd/pcmC4294967295D0p': No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a&amp;nbsp; /dev/snd/pcmC0D0p device, but obviously the 4294967295 is -1 because card in audio_hw_primary is -1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can connect audio via bluetooth, it works well, and there is no more error in logcat, however we will not always have a BT speaker connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I have to change something in audio_policy.conf ? How to remove this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 12:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-android-w-o-HW-sound/m-p/304528#M38885</guid>
      <dc:creator>frédéric</dc:creator>
      <dc:date>2014-03-26T12:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: using android w/o HW sound</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-android-w-o-HW-sound/m-p/304529#M38886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you need to modified hardware/imx to remove sound card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 13:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-android-w-o-HW-sound/m-p/304529#M38886</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-03-26T13:43:36Z</dc:date>
    </item>
  </channel>
</rss>