<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Issue: Udev events not generated by Ethernet driver</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304277#M38837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I was away and couldn't able to work on this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Udev Rules used:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx28evk:~# cat /etc/udev/rules.d/autonet.rules&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;# Handle network interface setup&lt;/P&gt;&lt;P&gt;SUBSYSTEM=="net", ACTION=="add" RUN+="/etc/udev/scripts/network.sh"&lt;/P&gt;&lt;P&gt;SUBSYSTEM=="net", ACTION=="remove" RUN+="/etc/udev/scripts/network.sh"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using opensource program in c to listen to all netlink activites from Kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking Netlink Activities from Kernel: &lt;STRONG&gt;netlink.c&lt;/STRONG&gt; (&lt;A href="http://pastebin.com/CA8NThAS"&gt;http://pastebin.com/CA8NThAS&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested with the latest kernel 2.6.35 and didnt found Ethernet plug/unplug event working. Find the below logs:&lt;/P&gt;&lt;P&gt;root@imx28evk:~# uname -r&lt;/P&gt;&lt;P&gt;2.6.35.3-1.1.0+yocto+g914558e&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx28evk:~# ./netlink&lt;/P&gt;&lt;P&gt;PHY: 0:00 - Link is Down&lt;/P&gt;&lt;P&gt;PHY: 0:00 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Same Program Works for USB Plug/Unplug events:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@imx28evk:~# ./netlink&lt;/P&gt;&lt;P&gt;usb 2-1: new high speed USB device using fsl-ehci and address 2&lt;/P&gt;&lt;P&gt;add@/devices/platform/fsl-ehci.0/usb2/2-1&lt;/P&gt;&lt;P&gt;ACTION=add&lt;/P&gt;&lt;P&gt;DEVPATH=/devices/platform/fsl-ehcscsi0 : usb-storage 2-1:1.0&lt;/P&gt;&lt;P&gt;i.0/usb2/2-1&lt;/P&gt;&lt;P&gt;SUBSYSTEM=usb&lt;/P&gt;&lt;P&gt;MAJOR=189&lt;/P&gt;&lt;P&gt;MINOR=129&lt;/P&gt;&lt;P&gt;DEVNAME=bus/usb/002/002&lt;/P&gt;&lt;P&gt;DEVTYPE=usb_device&lt;/P&gt;&lt;P&gt;PRODUCT=5dc/a817/1100&lt;/P&gt;&lt;P&gt;TYPE=0/0/0&lt;/P&gt;&lt;P&gt;BUSNUM=002&lt;/P&gt;&lt;P&gt;DEVNUM=002&lt;/P&gt;&lt;P&gt;SEQNUM=1830&lt;/P&gt;&lt;P&gt;add@/devices/platform/fsl-ehci.0/usb2/2-1/2-1:1.0&lt;/P&gt;&lt;P&gt;ACTION=add&lt;/P&gt;&lt;P&gt;DEVPATH=/devices/platform/fsl-ehci.0/usb2/2-1/2-1:1.0&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone throw some light on why Ethernet driver fails to send the plug/unplug event to udev via netlink sockets?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please feel free to share if you need more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jun 2014 03:04:34 GMT</pubDate>
    <dc:creator>B_K_Ankur</dc:creator>
    <dc:date>2014-06-10T03:04:34Z</dc:date>
    <item>
      <title>Issue: Udev events not generated by Ethernet driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304275#M38835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Friends,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.mx28evk with kernel 3.10.32 mainline on the board. I am facing issue of udev not receiving the events from Ethernet driver. I tried to monitor the udev events using command :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx28evk:~# udevadm monitor&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;custom logging function 0x17b9c registered&lt;/P&gt;&lt;P&gt;runtime dir '/var/run/udev'&lt;/P&gt;&lt;P&gt;calling: monitor&lt;/P&gt;&lt;P&gt;monitor will print the received events for:&lt;/P&gt;&lt;P&gt;UDEV - the event which udev sends out after rule processing&lt;/P&gt;&lt;P&gt;KERNEL - the kernel uevent&lt;/P&gt;&lt;P&gt;[ 5772.113167] libphy: 800f0000.etherne:00 - Link is Down&lt;/P&gt;&lt;P&gt;[ 5774.193557] libphy: 800f0000.etherne:00 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;//NO UDEV Events noticed disconnecting/connecting Ethernet 0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I do plug/unplug the USB mass storgage I got lots of messages with udev events including action = add/remove. But with ethernet plugging/unplugging, I am not getting any messages.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also tried to find in the driver source under linux/driver/net/ethernet/freescale but couldnt able to find any api used to send uevent via kobject. Any comments on how to enable the udev events for Ethernet driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 05:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304275#M38835</guid>
      <dc:creator>B_K_Ankur</dc:creator>
      <dc:date>2014-03-26T05:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: Issue: Udev events not generated by Ethernet driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304276#M38836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you share the udev rule? Have you tried this with the image of the FSL web page? (LTIB)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 23:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304276#M38836</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-03-31T23:13:41Z</dc:date>
    </item>
    <item>
      <title>Re: Issue: Udev events not generated by Ethernet driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304277#M38837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alejandro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I was away and couldn't able to work on this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Udev Rules used:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx28evk:~# cat /etc/udev/rules.d/autonet.rules&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;# Handle network interface setup&lt;/P&gt;&lt;P&gt;SUBSYSTEM=="net", ACTION=="add" RUN+="/etc/udev/scripts/network.sh"&lt;/P&gt;&lt;P&gt;SUBSYSTEM=="net", ACTION=="remove" RUN+="/etc/udev/scripts/network.sh"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using opensource program in c to listen to all netlink activites from Kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking Netlink Activities from Kernel: &lt;STRONG&gt;netlink.c&lt;/STRONG&gt; (&lt;A href="http://pastebin.com/CA8NThAS"&gt;http://pastebin.com/CA8NThAS&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested with the latest kernel 2.6.35 and didnt found Ethernet plug/unplug event working. Find the below logs:&lt;/P&gt;&lt;P&gt;root@imx28evk:~# uname -r&lt;/P&gt;&lt;P&gt;2.6.35.3-1.1.0+yocto+g914558e&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@imx28evk:~# ./netlink&lt;/P&gt;&lt;P&gt;PHY: 0:00 - Link is Down&lt;/P&gt;&lt;P&gt;PHY: 0:00 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Same Program Works for USB Plug/Unplug events:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@imx28evk:~# ./netlink&lt;/P&gt;&lt;P&gt;usb 2-1: new high speed USB device using fsl-ehci and address 2&lt;/P&gt;&lt;P&gt;add@/devices/platform/fsl-ehci.0/usb2/2-1&lt;/P&gt;&lt;P&gt;ACTION=add&lt;/P&gt;&lt;P&gt;DEVPATH=/devices/platform/fsl-ehcscsi0 : usb-storage 2-1:1.0&lt;/P&gt;&lt;P&gt;i.0/usb2/2-1&lt;/P&gt;&lt;P&gt;SUBSYSTEM=usb&lt;/P&gt;&lt;P&gt;MAJOR=189&lt;/P&gt;&lt;P&gt;MINOR=129&lt;/P&gt;&lt;P&gt;DEVNAME=bus/usb/002/002&lt;/P&gt;&lt;P&gt;DEVTYPE=usb_device&lt;/P&gt;&lt;P&gt;PRODUCT=5dc/a817/1100&lt;/P&gt;&lt;P&gt;TYPE=0/0/0&lt;/P&gt;&lt;P&gt;BUSNUM=002&lt;/P&gt;&lt;P&gt;DEVNUM=002&lt;/P&gt;&lt;P&gt;SEQNUM=1830&lt;/P&gt;&lt;P&gt;add@/devices/platform/fsl-ehci.0/usb2/2-1/2-1:1.0&lt;/P&gt;&lt;P&gt;ACTION=add&lt;/P&gt;&lt;P&gt;DEVPATH=/devices/platform/fsl-ehci.0/usb2/2-1/2-1:1.0&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone throw some light on why Ethernet driver fails to send the plug/unplug event to udev via netlink sockets?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please feel free to share if you need more information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 03:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304277#M38837</guid>
      <dc:creator>B_K_Ankur</dc:creator>
      <dc:date>2014-06-10T03:04:34Z</dc:date>
    </item>
    <item>
      <title>Re: Issue: Udev events not generated by Ethernet driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304278#M38838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Added Patch into kernel to send the udev events to userspace.Please find the attached one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE class="source"&gt;---&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="7" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; net/core/Makefile | 1 +&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="8" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; net/core/uevent.c | 43 +++++++++++++++++++++++++++++++++++++++++++&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="9" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; 2 files changed, 44 insertions(+)&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="10" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; create mode 100644 net/core/uevent.c&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="11" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="12" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;diff --git a/net/core/Makefile b/net/core/Makefile&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="13" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;index b33b996..a2139a7 100644&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="14" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;--- a/net/core/Makefile&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="15" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+++ b/net/core/Makefile&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="16" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;@@ -22,3 +22,4 @@ obj-$(CONFIG_TRACEPOINTS) += net-traces.o&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="17" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; obj-$(CONFIG_NET_DROP_MONITOR) += drop_monitor.o&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="18" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; obj-$(CONFIG_NETWORK_PHY_TIMESTAMPING) += timestamping.o&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="19" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt; obj-$(CONFIG_NETPRIO_CGROUP) += netprio_cgroup.o&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="20" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+obj-$(CONFIG_HOTPLUG) += uevent.o&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="21" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;diff --git a/net/core/uevent.c b/net/core/uevent.c&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="22" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;new file mode 100644&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="23" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;index 0000000..14b1e6e&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="24" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;--- /dev/null&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="25" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+++ b/net/core/uevent.c&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="26" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;@@ -0,0 +1,43 @@&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="27" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+/*&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="28" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ * Linux network device event notification&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="29" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ */&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="30" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="31" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+#include &amp;lt;linux/kernel.h&amp;gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="32" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+#include &amp;lt;linux/netdevice.h&amp;gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="33" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+#include &amp;lt;linux/kobject.h&amp;gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="34" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+#include &amp;lt;linux/notifier.h&amp;gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="35" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="36" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+/*&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="37" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ * Generate uevent in response to network device state changes.&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="38" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ * Other events are already handled by device subsystem.&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="39" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ */&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="40" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+static int netdev_event(struct notifier_block *this, unsigned long event,&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="41" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ void *ptr)&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="42" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+{&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="43" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ struct net_device *netdev = ptr;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="44" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="45" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ switch (event) {&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="46" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ case NETDEV_UP:&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="47" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ kobject_uevent(&amp;amp;netdev-&amp;gt;dev.kobj, KOBJ_ADD);&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="48" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ break;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="49" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ case NETDEV_DOWN:&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="50" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ kobject_uevent(&amp;amp;netdev-&amp;gt;dev.kobj, KOBJ_REMOVE);&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="51" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ break;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="52" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ case NETDEV_CHANGE:{&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="53" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ kobject_uevent(&amp;amp;netdev-&amp;gt;dev.kobj, KOBJ_CHANGE);&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="54" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ break;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="55" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ }&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="56" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ }&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="57" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ return NOTIFY_DONE;&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="58" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+}&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="59" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="60" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+static struct notifier_block netdev_uevent_notifier = {&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="61" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ .notifier_call = netdev_event,&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="62" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+};&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="63" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="64" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+static int __init netdev_uevent_init(void)&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="65" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+{&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="66" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+ return register_netdevice_notifier(&amp;amp;netdev_uevent_notifier);&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="67" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+}&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="68" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="69" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;+device_initcall(netdev_uevent_init);&lt;/CODE&gt;&lt;/P&gt;&lt;P class="line added-lines" data-line="70" data-line-type="ADDED"&gt;&lt;CODE class="source"&gt;-- &lt;/CODE&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 05:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304278#M38838</guid>
      <dc:creator>B_K_Ankur</dc:creator>
      <dc:date>2014-06-16T05:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: Issue: Udev events not generated by Ethernet driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304279#M38839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delay, it seems that you already solved the problem. Thanks a lot for sharing the solution!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2014 21:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-Udev-events-not-generated-by-Ethernet-driver/m-p/304279#M38839</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-06-18T21:33:06Z</dc:date>
    </item>
  </channel>
</rss>