<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304051#M38810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Grace,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use dd from the imx23 and copy the /boot/imx23_linux.sb with the corresponding offsets to the mmcblk0p1 in this case.&lt;/P&gt;&lt;P&gt;It did not work, It thought it must work but it did not.&lt;/P&gt;&lt;P&gt;One of the possible ways I use to think&amp;nbsp; that Zeki could use was to use TFTP to get the new .sb file and then just dd to replace the older one.&lt;/P&gt;&lt;P&gt;Can you provide more details about the correct procedure?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Mar 2014 21:42:32 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2014-03-31T21:42:32Z</dc:date>
    <item>
      <title>How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new image?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304048#M38807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How could I safely upgrade a Linux kernel image (imx28_ivt_linux.sb) remotely on a reference imx28 board. &lt;/P&gt;&lt;P&gt;What are my options? E.g. dual partition and dual kernel images? Copy the new kernel to a new directory and able to pint to it for booting? ...&lt;/P&gt;&lt;P&gt;Linux kernel version is 2.6.35.3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Mar 2014 21:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304048#M38807</guid>
      <dc:creator>zekibulbul</dc:creator>
      <dc:date>2014-03-25T21:22:39Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304049#M38808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can't run imx_ivt_linux.sb from a running kernel. Because imx_ivt_linux.sb includes 4 images which be loaded by ROM and run sequentially.&amp;nbsp; you can reference imx-bootlets-src-2.6.35.3-1.1.0/linux_ivt.bd. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 02:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304049#M38808</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2014-03-31T02:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304050#M38809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the response. I see that linux_ivt.bd calls power_prep, sdram_prep, linux_prep and then loads zImage and jumps to0x8000. Can the linux_ivt.bd script updated at runtime and e.g. change the zImage path and reboot? How about using kexec? Would loading a new zimage with kexec-l and then executing the new kernel with kexec -e work?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 16:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304050#M38809</guid>
      <dc:creator>zekibulbul</dc:creator>
      <dc:date>2014-03-31T16:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304051#M38810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Grace,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use dd from the imx23 and copy the /boot/imx23_linux.sb with the corresponding offsets to the mmcblk0p1 in this case.&lt;/P&gt;&lt;P&gt;It did not work, It thought it must work but it did not.&lt;/P&gt;&lt;P&gt;One of the possible ways I use to think&amp;nbsp; that Zeki could use was to use TFTP to get the new .sb file and then just dd to replace the older one.&lt;/P&gt;&lt;P&gt;Can you provide more details about the correct procedure?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Mar 2014 21:42:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304051#M38810</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2014-03-31T21:42:32Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304052#M38811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Linux_ivt.bd script is for ROM. "load" "jump" are all ROM commands.&lt;/P&gt;&lt;P&gt;kexec can be used to load kernel image on runtime. But unfortunately kexec can't work well in i.mx28 2.6.35.3 kernel. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 03:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304052#M38811</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2014-04-01T03:05:48Z</dc:date>
    </item>
    <item>
      <title>Re: How can I upgrade Linux kernel remotely uploading a new Linux kernel version on an i.mx28 reference board. Running Linux kernel 2.6.35.3. Can I copy a new imx28_ivt_linux.sb without overwriting the existing one onto the board and boot into this new im</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304053#M38812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For MX23, follow below steps to create SD card for boot. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. run fdisk /dev/sdb to create partition like below. the type of partition 2 is 53.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Disk /dev/sdb: 1977 MB, 1977614336 bytes&lt;/P&gt;&lt;P&gt;61 heads, 62 sectors/track, 1021 cylinders&lt;/P&gt;&lt;P&gt;Units = cylinders of 3782 * 512 = 1936384 bytes&lt;/P&gt;&lt;P&gt;Sector size (logical/physical): 512 bytes / 512 bytes&lt;/P&gt;&lt;P&gt;I/O size (minimum/optimal): 512 bytes / 512 bytes&lt;/P&gt;&lt;P&gt;Disk identifier: 0xa9280686&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Device Boot&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Start&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; End&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Blocks&amp;nbsp;&amp;nbsp; Id&amp;nbsp; System&lt;/P&gt;&lt;P&gt;/dev/sdb1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 18&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 34007&amp;nbsp;&amp;nbsp;&amp;nbsp; b&amp;nbsp; W95 FAT32&lt;/P&gt;&lt;P&gt;/dev/sdb2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 19&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 36&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 34038&amp;nbsp;&amp;nbsp; 53&amp;nbsp; OnTrack DM6 Aux3&lt;/P&gt;&lt;P&gt;/dev/sdb3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 37&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1021&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1862635&amp;nbsp;&amp;nbsp; 83&amp;nbsp; Linux&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. &lt;/P&gt;&lt;P&gt;sudo dd if=/dev/zero of=mmc_boot_partition.raw bs=512 count=4&lt;/P&gt;&lt;P&gt;sudo dd if=imx23_linux.sb of=mmc_boot_partition.raw ibs=512 seek=4 conv=sync,notrunc&lt;/P&gt;&lt;P&gt;sudo dd if=mmc_boot_partition.raw of=/dev/sdb2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. copy rootfs to partition 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 03:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-upgrade-Linux-kernel-remotely-uploading-a-new-Linux/m-p/304053#M38812</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2014-04-01T03:24:47Z</dc:date>
    </item>
  </channel>
</rss>