<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックemmc 4.4/4.5 device tree</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/emmc-4-4-4-5-device-tree/m-p/304016#M38794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an emmc with version 4.4/4.5 on my board.&lt;/P&gt;&lt;P&gt;How can I change the dts file to support the higher rate (I assume it just uses the "normal" rate if I don't tell it to use a higher rate or DDR)?&lt;/P&gt;&lt;P&gt;Or is this something I need to change in the code instead?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is it possible to boot this device from the i.MX6, since it's using version emmc 4.5 (what is the difference between 4,4 and 4.5 when it comes to boot)&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I populate the image in my flash, what is the best way?&lt;/P&gt;&lt;P&gt;Right now I tried to use the .sdcard file with dd, or do I need to do it in a different way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Apr 2014 16:41:53 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2014-04-25T16:41:53Z</dc:date>
    <item>
      <title>emmc 4.4/4.5 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/emmc-4-4-4-5-device-tree/m-p/304016#M38794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an emmc with version 4.4/4.5 on my board.&lt;/P&gt;&lt;P&gt;How can I change the dts file to support the higher rate (I assume it just uses the "normal" rate if I don't tell it to use a higher rate or DDR)?&lt;/P&gt;&lt;P&gt;Or is this something I need to change in the code instead?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is it possible to boot this device from the i.MX6, since it's using version emmc 4.5 (what is the difference between 4,4 and 4.5 when it comes to boot)&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I populate the image in my flash, what is the best way?&lt;/P&gt;&lt;P&gt;Right now I tried to use the .sdcard file with dd, or do I need to do it in a different way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Apr 2014 16:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/emmc-4-4-4-5-device-tree/m-p/304016#M38794</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-04-25T16:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: emmc 4.4/4.5 device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/emmc-4-4-4-5-device-tree/m-p/304017#M38795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Niklas,&lt;/P&gt;&lt;P&gt;from i.MX6Q and i.MX6DL RM: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;only support eMMC4.4.1, not support 4.5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Differencies are significant, you can read them in emmc specs documents.&lt;/P&gt;&lt;P&gt;However BSP supports basic read/write from eMMC 4.5 bypassing eMMC version checking,&lt;/P&gt;&lt;P&gt;so that eMMC v4.5 can work on current kernel as eMMC v4.4 cards, no specific v4.5 feature supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/u-mobo/linux-imx/commit/1aa14468261e300c4b912f2b400ac18976f61c7f" title="https://github.com/u-mobo/linux-imx/commit/1aa14468261e300c4b912f2b400ac18976f61c7f"&gt;ENGR00234519 mmc: support eMMC v4.5 memory cards · 1aa1446 · u-mobo/linux-imx · GitHub&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Higher rate or DDR are supported by driver automatically reading eMMC CSD register,&lt;/P&gt;&lt;P&gt;no need for additional configurations.&lt;/P&gt;&lt;P&gt;Populating image to flash is described in i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf&lt;/P&gt;&lt;P&gt;document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation"&gt;L3.0.35_4.1.0_LINUX_DOCS&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;i.MX6Q: i.MX 6Quad Family of Applications Processors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Apr 2014 12:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/emmc-4-4-4-5-device-tree/m-p/304017#M38795</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-28T12:29:48Z</dc:date>
    </item>
  </channel>
</rss>