<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Single Synchronous EIM Access in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303797#M38754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Figures 12 and 13 of the i.MX6 Dual/Quad Applications Products for Industrial Products data sheet show single read and write synchronous accesses on the EIM bus.&amp;nbsp; Can someone explain how those are achieved?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I assume an AXI read or write with burst length of 1 and burst size of 2(for a 16 bit data bus) would cause a single read or write synchronous access?&amp;nbsp; I am accessing registers in an FPGA and do not want to burst any data to/from the registers - only read or write single data words.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Would accessing a non-cached uint16 cause the proper AXI access?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; And, is BL ignored if a single AXI access is used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Mar 2014 17:48:36 GMT</pubDate>
    <dc:creator>tom1</dc:creator>
    <dc:date>2014-03-25T17:48:36Z</dc:date>
    <item>
      <title>Single Synchronous EIM Access</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303797#M38754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Figures 12 and 13 of the i.MX6 Dual/Quad Applications Products for Industrial Products data sheet show single read and write synchronous accesses on the EIM bus.&amp;nbsp; Can someone explain how those are achieved?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I assume an AXI read or write with burst length of 1 and burst size of 2(for a 16 bit data bus) would cause a single read or write synchronous access?&amp;nbsp; I am accessing registers in an FPGA and do not want to burst any data to/from the registers - only read or write single data words.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Would accessing a non-cached uint16 cause the proper AXI access?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; And, is BL ignored if a single AXI access is used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Mar 2014 17:48:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303797#M38754</guid>
      <dc:creator>tom1</dc:creator>
      <dc:date>2014-03-25T17:48:36Z</dc:date>
    </item>
    <item>
      <title>Re: Single Synchronous EIM Access</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303798#M38755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; Note, the Figures 12 and 13 of the Datasheet should be considered mainly as &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;demonstration material,where waveforms are used to show (emphasize) some &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;timing parameters. You are right, the waveforms correspond to burst length of 1,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;but note, the i.MX6 EIM does not allow it : minimal value for burst length BL is&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;4 beats.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Mar 2014 07:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303798#M38755</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-03-28T07:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: Single Synchronous EIM Access</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303799#M38756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK.&amp;nbsp; I will switch to asynchronous mode since single word transfers are impossible in synchronous mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 12:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303799#M38756</guid>
      <dc:creator>tom1</dc:creator>
      <dc:date>2014-04-02T12:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: Single Synchronous EIM Access</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303800#M38757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did the synchronous mode prove useful for audio data transfer over EIM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Abhijeet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 04:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Synchronous-EIM-Access/m-p/303800#M38757</guid>
      <dc:creator>abhijeet_ghodga</dc:creator>
      <dc:date>2020-03-03T04:11:46Z</dc:date>
    </item>
  </channel>
</rss>