<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6 Linux BSP support for System-80 LCDs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303290#M38638</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Attached is the system 80 LCD patch for iMX51 3DS board, maybe you can reference to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The panel is GPM722A0, the controller chip is ILI9320.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 May 2014 01:51:34 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2014-05-23T01:51:34Z</dc:date>
    <item>
      <title>iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303287#M38635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear experts--&lt;/P&gt;&lt;P&gt;I need to connect an LCD with a System-80 (Aka. Intel-80) to an iMX6 Solo (8-bit Async Parallel i/f)&lt;/P&gt;&lt;P&gt;According to the Reference Manual, the IPUv3 DI has support for this interface, but I read an old thread that the Linux BSP drivers do not include support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has this support be added in more recent releases?&lt;/P&gt;&lt;P&gt;Has anyone successfully connected a System-80 LCD to an IMX6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Erez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 08:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303287#M38635</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2014-05-22T08:24:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303288#M38636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no such driver on iMX6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 09:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303288#M38636</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-05-22T09:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303289#M38637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know of anyone here that has done that, but Qiang Li is right, there is no driver available, you would need to develop it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Sergio&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 14:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303289#M38637</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-05-22T14:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303290#M38638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Attached is the system 80 LCD patch for iMX51 3DS board, maybe you can reference to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The panel is GPM722A0, the controller chip is ILI9320.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 May 2014 01:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303290#M38638</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-05-23T01:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303291#M38639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;Do you know, which LCD interfaces have drivers in the iMX6 Linux BSP?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 11:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303291#M38639</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2014-05-26T11:57:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303292#M38640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any estimate how complicated it is to create such a driver for iMX6 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 11:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303292#M38640</guid>
      <dc:creator>erezsteinberg</dc:creator>
      <dc:date>2014-05-26T11:59:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Linux BSP support for System-80 LCDs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303293#M38641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think it is not an easy task, too less people knows the IPU ADC well.&lt;/P&gt;&lt;P&gt;Another choise, maybe you can use GPIO to simulate the system-80 signal, it will be more easy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 03:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Linux-BSP-support-for-System-80-LCDs/m-p/303293#M38641</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2014-05-29T03:39:46Z</dc:date>
    </item>
  </channel>
</rss>