<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Qt multimedia error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Qt-multimedia-error/m-p/303235#M38605</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And I've check the ../qt5/qtbase/mkspecs/modules&lt;/P&gt;&lt;P&gt;There's no file like qt_lib_multimedia.pri.&lt;/P&gt;&lt;P&gt;Is this the cause of the problem?&lt;/P&gt;&lt;P&gt;How can I install it back?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Apr 2014 17:12:04 GMT</pubDate>
    <dc:creator>yiniguo</dc:creator>
    <dc:date>2014-04-25T17:12:04Z</dc:date>
    <item>
      <title>Qt multimedia error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt-multimedia-error/m-p/303234#M38604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all:&lt;/P&gt;&lt;P&gt;I’m now trying to build a media player on a &lt;SPAN class="caps"&gt;ARM&lt;/SPAN&gt; board, the cpu is freescale iMX6. System on board is ubuntu 12.04. And I have build a cross compiler for the board on my PC which is also running 12.04.&lt;BR /&gt; I’ve built a small program using QSound to play a wav file successfully on my computer.&lt;BR /&gt; But when I tried to compile it with cross compiler, a notice reads: “ Project &lt;SPAN class="caps"&gt;ERROR&lt;/SPAN&gt;: Unknown module(s) in QT: multimedia “ appeared. &lt;BR /&gt; In my .pro file, I’ve added QT += widgets multimedia.&lt;BR /&gt; And I’ve include &amp;lt;QSound&amp;gt; in my main.cpp.&lt;BR /&gt; And I’ve checked the cross compiler libs, there’s QSound there. &lt;/P&gt;&lt;P&gt;When compile programs for PC, I use g++.&lt;BR /&gt; And for the arm system, I use arm-fsl-linux-gnueabi-gcc.&lt;/P&gt;&lt;P&gt;I build the Qt5 cross compiler according to the website:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="94066" data-objecttype="102" href="https://community.freescale.com/docs/DOC-94066"&gt;https://community.freescale.com/docs/DOC-94066&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So does anyone meet the same problem?&lt;BR /&gt; Do I need to set more parameters?&lt;BR /&gt; Thanks a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Apr 2014 01:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt-multimedia-error/m-p/303234#M38604</guid>
      <dc:creator>yiniguo</dc:creator>
      <dc:date>2014-04-25T01:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: Qt multimedia error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt-multimedia-error/m-p/303235#M38605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And I've check the ../qt5/qtbase/mkspecs/modules&lt;/P&gt;&lt;P&gt;There's no file like qt_lib_multimedia.pri.&lt;/P&gt;&lt;P&gt;Is this the cause of the problem?&lt;/P&gt;&lt;P&gt;How can I install it back?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Apr 2014 17:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt-multimedia-error/m-p/303235#M38605</guid>
      <dc:creator>yiniguo</dc:creator>
      <dc:date>2014-04-25T17:12:04Z</dc:date>
    </item>
  </channel>
</rss>