<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic V4l2 camera capture on imx6 cannot capture RGB24 correctly in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302969#M38489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using SabreSD imx6q evaluation board and trying to capture data with V4L2_PIX_FMT_RGB24, and it does seem to work when I use the ipu_prp_enc.c. driver, however when I use the ipu_csi_enc.c driver the colours are quite wrong?&lt;/P&gt;&lt;P&gt;I seem to be able to get correct colour if I use the V4L2_PIX_FMT_YUYV pixel format when using both drivers.&lt;/P&gt;&lt;P&gt;Is this a known issue. I using kernel L3.0.35.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 May 2014 23:28:06 GMT</pubDate>
    <dc:creator>makislivadas</dc:creator>
    <dc:date>2014-05-21T23:28:06Z</dc:date>
    <item>
      <title>V4l2 camera capture on imx6 cannot capture RGB24 correctly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302969#M38489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using SabreSD imx6q evaluation board and trying to capture data with V4L2_PIX_FMT_RGB24, and it does seem to work when I use the ipu_prp_enc.c. driver, however when I use the ipu_csi_enc.c driver the colours are quite wrong?&lt;/P&gt;&lt;P&gt;I seem to be able to get correct colour if I use the V4L2_PIX_FMT_YUYV pixel format when using both drivers.&lt;/P&gt;&lt;P&gt;Is this a known issue. I using kernel L3.0.35.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 23:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302969#M38489</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2014-05-21T23:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: V4l2 camera capture on imx6 cannot capture RGB24 correctly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302970#M38490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A href="https://community.nxp.com/space/2004"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 08:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302970#M38490</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-05-26T08:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: V4l2 camera capture on imx6 cannot capture RGB24 correctly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302971#M38491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have now build the latest Yocto based BSP with Linux 3.10.17 and the problem is still present.&lt;/P&gt;&lt;P&gt;It does seem to me that the ipu_csi_enc.c driver although it accepts V4L2_PIX_FMT_RGB24 capture format it does not seem able to support it properly. The only format that seems to work is V4L2_PIX_FMT_YUYV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 May 2014 21:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4l2-camera-capture-on-imx6-cannot-capture-RGB24-correctly/m-p/302971#M38491</guid>
      <dc:creator>makislivadas</dc:creator>
      <dc:date>2014-05-31T21:54:09Z</dc:date>
    </item>
  </channel>
</rss>