<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFG - Manufacturing Tool - i.mx6 - Fails when jumping to OS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302450#M38348</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a SabreSD board and I'm not able to complete the boot process with the MFG Tool and the MFG kernel.&lt;/P&gt;&lt;P&gt;Actually I'm using the "linux-imx-mfgtool-3.10.17" kernel provided by the latest version of bitbake from the branch master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems occur when going into the "jumping to OS" phase.&lt;/P&gt;&lt;P&gt;The uboot, kernel and initrd images are loaded correctly and the board is able to start the booting sequence.&lt;/P&gt;&lt;P&gt;At some point, the kernel display recursively "Waiting for UTP device" and the boot process stops.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The development machine runs Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I can do to try understanding where the problem is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 May 2014 07:55:40 GMT</pubDate>
    <dc:creator>ferrucciopaccia</dc:creator>
    <dc:date>2014-05-21T07:55:40Z</dc:date>
    <item>
      <title>MFG - Manufacturing Tool - i.mx6 - Fails when jumping to OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302450#M38348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a SabreSD board and I'm not able to complete the boot process with the MFG Tool and the MFG kernel.&lt;/P&gt;&lt;P&gt;Actually I'm using the "linux-imx-mfgtool-3.10.17" kernel provided by the latest version of bitbake from the branch master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems occur when going into the "jumping to OS" phase.&lt;/P&gt;&lt;P&gt;The uboot, kernel and initrd images are loaded correctly and the board is able to start the booting sequence.&lt;/P&gt;&lt;P&gt;At some point, the kernel display recursively "Waiting for UTP device" and the boot process stops.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The development machine runs Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything I can do to try understanding where the problem is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 07:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302450#M38348</guid>
      <dc:creator>ferrucciopaccia</dc:creator>
      <dc:date>2014-05-21T07:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: MFG - Manufacturing Tool - i.mx6 - Fails when jumping to OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302451#M38349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;H Ferrucio&lt;/P&gt;&lt;P&gt;please try&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;IMX_6_MFG_L3.10.17_1.0.0_TOOL&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : i.MX 6Family Manufacturing Toolkit for L3.10.17.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with images&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.10.17_1.0.0_IMX6QDLS_BUNDLE&lt;/A&gt; &lt;IMG alt="" class="jiveImage" src="http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif" /&gt; : Source Code Download Steps Documentation and Demo Images. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 May 2014 10:26:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302451#M38349</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-24T10:26:01Z</dc:date>
    </item>
    <item>
      <title>Re: MFG - Manufacturing Tool - i.mx6 - Fails when jumping to OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302452#M38350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In some occasions when the process halts at “jumping to OS” image it’s a problem related to the U-Boot file. Please make sure that the u-boot.bin being used by the profile is the appropriate for your board and let us know If this help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 15:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302452#M38350</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2014-05-29T15:44:36Z</dc:date>
    </item>
    <item>
      <title>Re: MFG - Manufacturing Tool - i.mx6 - Fails when jumping to OS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302453#M38351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ferruccio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to the other suggestions, two things to check:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. In the cfg.ini file, verify that the value for name matches the name entry you intended to use in ucl2.xml.&lt;/P&gt;&lt;P&gt;2. For the given name target, verify that each file entry matches up to an actual file with the correct filename in the proper location. You may just have a typo somewhere. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Robbeloth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 May 2014 16:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFG-Manufacturing-Tool-i-mx6-Fails-when-jumping-to-OS/m-p/302453#M38351</guid>
      <dc:creator>michaelrobbelot</dc:creator>
      <dc:date>2014-05-29T16:52:44Z</dc:date>
    </item>
  </channel>
</rss>