<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: WiFi / Ethernet coexistence in Android in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-coexistence-in-Android/m-p/301883#M38144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A _jive_internal="true" class="jivecontainerTT-hover-container jive-link-community-small" data-containerid="1" data-containertype="14" data-objectid="2004" data-objecttype="14" href="https://community.nxp.com/community/imx"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 May 2014 08:54:09 GMT</pubDate>
    <dc:creator>Wlodek_D_</dc:creator>
    <dc:date>2014-05-26T08:54:09Z</dc:date>
    <item>
      <title>WiFi / Ethernet coexistence in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-coexistence-in-Android/m-p/301882#M38143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see that in both ICS and JB WiFi and Ethernet cannot coexist.&lt;/P&gt;&lt;P&gt;I have quite figured out the reason: ConnectivityService.java manages kind of policy, where all the network connections are prioritized, so the one with the lower priority is torn down (Ethernet happens to be prioritized over WiFi).&lt;/P&gt;&lt;P&gt;When the unrequired network is disconnected (e.g. Ethernet cable is pulled out or WiFi is off), the other network is Ok.&lt;/P&gt;&lt;P&gt;But in order to use my device (i.mx6) as an access point, I would like to have them both.&lt;/P&gt;&lt;P&gt;I have tried to merely delete the policy checks from the code, but, at least with JB, it seems to screw the networking altogether.&lt;/P&gt;&lt;P&gt;How can it be done ?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Andrey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 15:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-coexistence-in-Android/m-p/301882#M38143</guid>
      <dc:creator>andreygelman</dc:creator>
      <dc:date>2014-05-20T15:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi / Ethernet coexistence in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-coexistence-in-Android/m-p/301883#M38144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A _jive_internal="true" class="jivecontainerTT-hover-container jive-link-community-small" data-containerid="1" data-containertype="14" data-objectid="2004" data-objecttype="14" href="https://community.nxp.com/community/imx"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; (&lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 May 2014 08:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Ethernet-coexistence-in-Android/m-p/301883#M38144</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-05-26T08:54:09Z</dc:date>
    </item>
  </channel>
</rss>